2D Graphic acceleration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2D Graphic acceleration

2,032件の閲覧回数
hirojiibaraki
Contributor I

Hi community,
Table2 of 12 pages in IMX6DQAEC Rev.2.3,07/2013 have description of GPU2Dv2.
Does i.mx6 have two or more graphic layers and Can it do a screen overlay?
Can Directdraw of WEC7 carry out hardware acceleration?
Can Flash player carry out hardware acceleration?
I would like to raise the grace of character scrolling.

Best Regards,
hiroji ibaraki

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,772件の閲覧回数
b36401
NXP Employee
NXP Employee

Actually Freescale itself does not support winCE environments for i.MX6.

There is a company that developed winCE for the i.MX6.

It is Adeneo Embedded:

www.adeneo-embedded.com

You can contact them in point of the details.

Irrespective of winCE, screen overlay is supported.

As for flash, you will need special NDA for getting flash player.

Please contact your local Freescale representative regarding this.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,772件の閲覧回数
hirojiibaraki
Contributor I

Thanks for your suggestion.

I will try to contact Freescale representative.

Best Regards.

ibaraki

From: Victor Linnik

Sent: Friday, April 18, 2014 5:44 PM

To: hiroji ibaraki

Subject: Re: - 2D Graphic acceleration

2D Graphic acceleration

reply from Victor Linnik in i.MX Community - View the full discussion

0 件の賞賛
返信