Hi NXP
We need to address the Year 2038 issue on the 32-bit i.MX6 CPU within our Yocto 4.2 Mickledore environment.
Do you have a solution?
We attempted to include "conf/distro/include/time64.inc" in "source/meta-advantech/meta-fsl-imx/conf/machine/include/advantech-imx6-settings.inc".
However, this resulted in build failures for fsl-gstreamer1.0 and imx-test.
Do you have any advice?
Thanks.
Thanks.
Hello @charleshuang
I hope you are doing well.
It seems that the issue was solved since the 5.6 kernel, as you can see here.
What BSP are you using?
Best regrads,
Salas.
Thanks for your feedback.
Our BSP is Yocto 4.2.
I think so the 6.1.22 kernel is already support it about fixed the 2038 year issue.
We need to add "time64.inc" in machine-settings.inc on Yocto.
But we try add it, some packages(fsl-gstreamer1.0-full, imx-test and fsl-tools-testapps,) will be build fail .
Do you have any advice?
Thanks.