通过BT656、BT1120总线的方式,输入720P的图像;时钟频率在148.5MHz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

通过BT656、BT1120总线的方式,输入720P的图像;时钟频率在148.5MHz

跳至解决方案
3,668 次查看
shunwenyu
Contributor I

应用需求:   

  1.   通过BT656、BT1120总线的方式,输入720P的图像;时钟信号在148.5MHz   

  2.  处理器用I.MX535   

  这个方案可行吗 

标签 (1)
0 项奖励
回复
1 解答
2,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shunwen

yes i.MX53 can support 720p BT656 camera input, performance is given in

IMX53RM sect.45.3.1.1 Camera Ports

The input rate supported by the camera port is as follows:

Average: up to 135M values/sec Bayer - 90 M pixels/sec (e.g., 9M pixels @ 15

fps) YUV 4:2:2 - 45 M pixels/sec (e.g., 3M pixels @ 15 fps) YUV 4:4:4 or RGB

- 30 M pixels/sec (e.g., 3M pixels @ 10 fps)

• Peak: up to 180 values/sec (to account for up to 35% blanking intervals)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,691 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shunwen

yes i.MX53 can support 720p BT656 camera input, performance is given in

IMX53RM sect.45.3.1.1 Camera Ports

The input rate supported by the camera port is as follows:

Average: up to 135M values/sec Bayer - 90 M pixels/sec (e.g., 9M pixels @ 15

fps) YUV 4:2:2 - 45 M pixels/sec (e.g., 3M pixels @ 15 fps) YUV 4:4:4 or RGB

- 30 M pixels/sec (e.g., 3M pixels @ 10 fps)

• Peak: up to 180 values/sec (to account for up to 35% blanking intervals)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复