通过BT656、BT1120总线的方式,输入720P的图像;时钟频率在148.5MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

通过BT656、BT1120总线的方式,输入720P的图像;时钟频率在148.5MHz

Jump to solution
3,089 Views
shunwenyu
Contributor I

应用需求:   

  1.   通过BT656、BT1120总线的方式,输入720P的图像;时钟信号在148.5MHz   

  2.  处理器用I.MX535   

  这个方案可行吗 

Labels (1)
0 Kudos
1 Solution
2,111 Views
igorpadykov
NXP Employee
NXP Employee

Hi shunwen

yes i.MX53 can support 720p BT656 camera input, performance is given in

IMX53RM sect.45.3.1.1 Camera Ports

The input rate supported by the camera port is as follows:

Average: up to 135M values/sec Bayer - 90 M pixels/sec (e.g., 9M pixels @ 15

fps) YUV 4:2:2 - 45 M pixels/sec (e.g., 3M pixels @ 15 fps) YUV 4:4:4 or RGB

- 30 M pixels/sec (e.g., 3M pixels @ 10 fps)

• Peak: up to 180 values/sec (to account for up to 35% blanking intervals)

Best regards

igor
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
2,112 Views
igorpadykov
NXP Employee
NXP Employee

Hi shunwen

yes i.MX53 can support 720p BT656 camera input, performance is given in

IMX53RM sect.45.3.1.1 Camera Ports

The input rate supported by the camera port is as follows:

Average: up to 135M values/sec Bayer - 90 M pixels/sec (e.g., 9M pixels @ 15

fps) YUV 4:2:2 - 45 M pixels/sec (e.g., 3M pixels @ 15 fps) YUV 4:4:4 or RGB

- 30 M pixels/sec (e.g., 3M pixels @ 10 fps)

• Peak: up to 180 values/sec (to account for up to 35% blanking intervals)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos