关于System PLL的问题!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

关于System PLL的问题!

676件の閲覧回数
yangweihuadiand
Contributor I

关于System PLL的问题!

在IMX6DQRM Rev. 3中部分章节对System PLL为:

PLL2 (also referred tp as System_PLL or 528_PLL)

即PLL2又称为System PLL。

Chapter 18 Clock Controller Module (CCM)对System PLL有专门的描述:

PLL2 also referenced as System PLL

但在Chapter 8 System Boot 一章中的8.4.3 Clocks at Boot Time 

Table 8-4. Normal Frequency Clocks Configuration

160477_160477.pngpastedImage_1.png

 

上表中,显然System PLL来自pll1,为ARM Core  clock的前级时钟(ARM Core固定2分频前的时钟)

这就让我很疑惑System PLL到底为何?

谢谢!

ラベル(1)
0 件の賞賛
返信
1 返信

604件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Sorry, the Table 8-4 is a bit confused.

In this table 8-4, the "System PLL" is the ARM PLL , the "528MHz PLL" is the System PLL which mentioned in Chapter 18.5.1.3 PLL reference clock.

0 件の賞賛
返信