关于System PLL的问题!
在IMX6DQRM Rev. 3中部分章节对System PLL为:
PLL2 (also referred tp as System_PLL or 528_PLL)
即PLL2又称为System PLL。
Chapter 18 Clock Controller Module (CCM)对System PLL有专门的描述:
PLL2 also referenced as System PLL
但在Chapter 8 System Boot 一章中的8.4.3 Clocks at Boot Time
Table 8-4. Normal Frequency Clocks Configuration
上表中,显然System PLL来自pll1,为ARM Core clock的前级时钟(ARM Core固定2分频前的时钟)
这就让我很疑惑System PLL到底为何?
谢谢!
Sorry, the Table 8-4 is a bit confused.
In this table 8-4, the "System PLL" is the ARM PLL , the "528MHz PLL" is the System PLL which mentioned in Chapter 18.5.1.3 PLL reference clock.