In our daily work as a FAE (Field Application Engineer), we need to read and write to SD cards, and often this requires working under Windows. The Win32 Disk Imager tool provides this functionality, but it cannot specify a particular offset or dump a mirror based on the disk partition size. After dumping the disk mirror, if it's a GPT (Global Point of View) system, we also need to repair the backup GPT table. This prompted me to write dedicated tools.
I'm currently using the tools myself and hope to share them to bring some convenience to the daily work.
It's recommended to place the tools in the Windows path, so it can be run from anywhere.
Author: Biyong SUN
Version: 1.0.6
Introduction:
RawDisk Menu Tool is an advanced Windows utility for low-level disk operations on removable drives (such as SD cards and USB drives). Unlike traditional tools like Win32 Disk Imager, which can only write from offset 0 and dump the entire disk, RawDisk Menu offers fine-grained control over disk access:
Flexible Offsets:
0.Custom Lengths:
Block Size Control:
Dry-Run Mode:
Partition Awareness:
Safety Features:
Workflow Highlights:
| Feature | RawDisk Menu Tool | Win32 Disk Imager |
| Platform | Windows | Windows |
| Read Disk to Image | Yes (supports partial reads) | Yes (entire disk only) |
| Write Image to Disk | Yes (supports partial writes) | Yes (entire disk only) |
| Offset Control | Any offset (customizable) | Fixed at 0 |
| Length Control | Custom length (partial disk or partition) | Entire disk only |
| Block Size Control | Configurable (up to 50 MB, multiple of 512) | Fixed (no user control) |
| Dry-Run Mode | Yes (preview without writing) | No |
| Partition Awareness | Displays partition layout and metadata | No |
| Disk Size Limit | Configurable (default 128 GB) | No limit (but entire disk only) |
| Safety Features | Locks/dismounts volumes before write | No |
| Progress Display | Yes (with percentage) | Yes |
| Hex/ASCII Preview | Yes (first 32 bytes in dry-run) | No |
| Use Case | Advanced: selective backup/restore, forensic work | Basic: full disk imaging only |
Author: Biyong SUN
Version: 1.0.3
Purpose:
This tool is designed for analyzing and repairing disk image files, particularly focusing on partition structures and GPT (GUID Partition Table) integrity. Its main capabilities include:
Partition Detection:
GPT Backup Repair:
Disk Information Display:
Usage Highlights:
-s or --show: Display disk info only.-f or --fix: Repair GPT backup and then display disk info.This batch file can help you get the admin for this directory in the File Explorer address bar.
type cmda in the File Explorer address bar.
C:\Windows\System32\cmda.bat
@echo off
:: Check for admin rights
net session >nul 2>&1
if %errorlevel% == 0 (
echo Already running as administrator.
cmd
exit /b
) else (
echo Requesting administrator privileges...
powershell -Command "Start-Process cmd.exe -Verb runAs"
exit /b
)
``