Patch to support BlueTooth on iMX6SL EVK board, Android JB4.3 GA1.1.0 BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Patch to support BlueTooth on iMX6SL EVK board, Android JB4.3 GA1.1.0 BSP

Patch to support BlueTooth on iMX6SL EVK board, Android JB4.3 GA1.1.0 BSP

For default Android JB4.3 GA1.1.0 BSP, iMX6SL EVK board doesn't support BlueTooth, attached is the patch for the BSP to support AR3002 bluetooth.

 

The hardware information can be found at: https://community.freescale.com/docs/DOC-95016

 

iMX6SL_EVK_BlueTooth_Patch_for_JB4.3_1.1.0.tar.gz: these are the patch files.

iMX6SL_EVK_BlueTooth_Support_for_JB4.3_1.1.0.tar.gz: these are the patched source code files.

Please select one of above to use.

Attachments
Comments

Hi All,

My platform is IMX6SL, Android kitkat 4.4.3 , Bluedroid, bluetooth USB driver.

When I am inserting my ko from the GUI, it is giving this error,

Can you please suggest me what to do???

Unable to unload driver module "/system/bin/bluetooth.ko": Operation not permitted

************* bluetooth.c insmod is called**********

Failed to load module: Unknown error -1 (-1)

                                                 

I think it's purely permissions issue,

Here I have few questions,

1. Is the path which I am placing my kernel object file (ko) above /system/bin/release/ is correct ?? or it is /data/misc/bluetooth/ path???

2. If it is /data/misc/bluetooth/ then where should I mention permissions for that path.

Please respond me,

Thanks and Regards,

Mutyala rao.

For USB bluetooth, you can reference to this discussion:

Re: USB support in Bluedroid stack [Android 4.4.3 for imx6-Sololite]

No ratings
Version history
Last update:
‎06-06-2014 01:39 AM
Updated by: