PPS on i.MX 93 EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PPS on i.MX 93 EVK

PPS on i.MX 93 EVK

Introduction

Time Synchronization stands for the alignment of time within distributed nodes, pretty critical for real-time applications, control and measurement systems as voice and video networks; all of them being embedded applications.

It needs the synchronization of frequency, phase and time between all the nodes and offers action coordination, high precision triggers and event reference or timestamping. [1]

A Time Synchronization resource it's the ethernet standard for time PTP or IEEE 1588 standard, its study begin with the physical representation of time information: PPS; Pulse Per Second.

An squared wave timed by the capable MACs, in i.MX families we have two MACs of which.

Background

Customers are interested in this signal, we have an i.MX 8M Plus kernel 5 resource but there is a new processor family using the next major kernel version; 6. [2]

We will go through demonstrating PPS on i.MX 93 EVK in both MACs; FEC and EQOS.

HW setup

  • i.MX 93 EVK boot over eMMC.
  • Connect power and debug receptacles.

Hands-on for FEC or eth0 MAC

uSDHC2 pin group conflicts with the pps output pin and you are ought to remove the uSDHC2 nodes and assign the event0 out pin to the FEC pin group as shown below.

--- imx93-11x11-evk.dts 2024-08-23 18:19:56.344798901 +0200
+++ imx93-11x11-evk-pps.dts     2024-09-02 21:31:46.569477421 +0200
@@ -100,18 +100,6 @@
        regulator-max-microvolt = <1800000>;
    };
 
-   reg_usdhc2_vmmc: regulator-usdhc2 {
-       compatible = "regulator-fixed";
-       pinctrl-names = "default";
-       pinctrl-0 = <&pinctrl_reg_usdhc2_vmmc>;
-       regulator-name = "VSD_3V3";
-       regulator-min-microvolt = <3300000>;
-       regulator-max-microvolt = <3300000>;
-       gpio = <&gpio3 7 GPIO_ACTIVE_HIGH>;
-       off-on-delay-us = <12000>;
-       enable-active-high;
-   };
-
    reg_vdd_12v: regulator-vdd-12v {
        compatible = "regulator-fixed";
        regulator-name = "reg_vdd_12v";
@@ -770,21 +766,6 @@
    status = "okay";
};

-&usdhc2 {
-   pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep";
-   pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>;
-   pinctrl-1 = <&pinctrl_usdhc2_100mhz>, <&pinctrl_usdhc2_gpio>;
-   pinctrl-2 = <&pinctrl_usdhc2_200mhz>, <&pinctrl_usdhc2_gpio>;
-   pinctrl-3 = <&pinctrl_usdhc2_sleep>, <&pinctrl_usdhc2_gpio_sleep>;
-   cd-gpios = <&gpio3 00 GPIO_ACTIVE_LOW>;
-   fsl,cd-gpio-wakeup-disable;
-   vmmc-supply = <&reg_usdhc2_vmmc>;
-   bus-width = <4>;
-   status = "okay";
-   no-sdio;
-   no-mmc;
-};
-
 &usdhc3 {
    pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep";
    pinctrl-0 = <&pinctrl_usdhc3>, <&pinctrl_usdhc3_wlan>;
@@ -860,14 +842,15 @@
            MX93_PAD_ENET2_RD1__ENET1_RGMII_RD1             0x57e
            MX93_PAD_ENET2_RD2__ENET1_RGMII_RD2             0x57e
            MX93_PAD_ENET2_RD3__ENET1_RGMII_RD3             0x57e
            MX93_PAD_ENET2_RXC__ENET1_RGMII_RXC             0x58e
            MX93_PAD_ENET2_RX_CTL__ENET1_RGMII_RX_CTL       0x57e
            MX93_PAD_ENET2_TD0__ENET1_RGMII_TD0             0x57e
            MX93_PAD_ENET2_TD1__ENET1_RGMII_TD1             0x57e
            MX93_PAD_ENET2_TD2__ENET1_RGMII_TD2             0x57e
            MX93_PAD_ENET2_TD3__ENET1_RGMII_TD3             0x57e
            MX93_PAD_ENET2_TXC__ENET1_RGMII_TXC             0x58e
            MX93_PAD_ENET2_TX_CTL__ENET1_RGMII_TX_CTL       0x57e
+           MX93_PAD_SD2_DATA0__ENET1_1588_EVENT0_OUT       0x31e
        >;
    };

@@ -887,6 +870,7 @@
            MX93_PAD_ENET2_TD3__GPIO4_IO16                  0x51e
            MX93_PAD_ENET2_TXC__GPIO4_IO21                  0x51e
            MX93_PAD_ENET2_TX_CTL__GPIO4_IO20               0x51e
+           MX93_PAD_SD2_DATA0__GPIO3_IO03                  0x31e
        >;
    };

@@ -998,75 +982,6 @@
        >;
    };

-   pinctrl_reg_usdhc2_vmmc: regusdhc2vmmcgrp {
-       fsl,pins = <
-           MX93_PAD_SD2_RESET_B__GPIO3_IO07        0x31e
-       >;
-   };
-
-   pinctrl_usdhc2_gpio: usdhc2gpiogrp {
-       fsl,pins = <
-           MX93_PAD_SD2_CD_B__GPIO3_IO00           0x31e
-       >;
-   };
-
-   pinctrl_usdhc2_gpio_sleep: usdhc2gpiogrpsleep {
-       fsl,pins = <
-           MX93_PAD_SD2_CD_B__GPIO3_IO00           0x51e
-       >;
-   };
-
-   /* need to config the SION for data and cmd pad, refer to ERR052021 */
-   pinctrl_usdhc2: usdhc2grp {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__USDHC2_CLK            0x1582
-           MX93_PAD_SD2_CMD__USDHC2_CMD            0x40001382
-           MX93_PAD_SD2_DATA0__USDHC2_DATA0        0x40001382
-           MX93_PAD_SD2_DATA1__USDHC2_DATA1        0x40001382
-           MX93_PAD_SD2_DATA2__USDHC2_DATA2        0x40001382
-           MX93_PAD_SD2_DATA3__USDHC2_DATA3        0x40001382
-           MX93_PAD_SD2_VSELECT__USDHC2_VSELECT    0x51e
-       >;
-   };
-
-   /* need to config the SION for data and cmd pad, refer to ERR052021 */
-   pinctrl_usdhc2_100mhz: usdhc2-100mhzgrp {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__USDHC2_CLK            0x158e
-           MX93_PAD_SD2_CMD__USDHC2_CMD            0x4000138e
-           MX93_PAD_SD2_DATA0__USDHC2_DATA0        0x4000138e
-           MX93_PAD_SD2_DATA1__USDHC2_DATA1        0x4000138e
-           MX93_PAD_SD2_DATA2__USDHC2_DATA2        0x4000138e
-           MX93_PAD_SD2_DATA3__USDHC2_DATA3        0x4000138e
-           MX93_PAD_SD2_VSELECT__USDHC2_VSELECT    0x51e
-       >;
-   };
-
-   /* need to config the SION for data and cmd pad, refer to ERR052021 */
-   pinctrl_usdhc2_200mhz: usdhc2-200mhzgrp {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__USDHC2_CLK            0x15fe
-           MX93_PAD_SD2_CMD__USDHC2_CMD            0x400013fe
-           MX93_PAD_SD2_DATA0__USDHC2_DATA0        0x400013fe
-           MX93_PAD_SD2_DATA1__USDHC2_DATA1        0x400013fe
-           MX93_PAD_SD2_DATA2__USDHC2_DATA2        0x400013fe
-           MX93_PAD_SD2_DATA3__USDHC2_DATA3        0x400013fe
-           MX93_PAD_SD2_VSELECT__USDHC2_VSELECT    0x51e
-       >;
-   };
-
-   pinctrl_usdhc2_sleep: usdhc2grpsleep {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__GPIO3_IO01            0x51e
-           MX93_PAD_SD2_CMD__GPIO3_IO02            0x51e
-           MX93_PAD_SD2_DATA0__GPIO3_IO03          0x51e
-           MX93_PAD_SD2_DATA1__GPIO3_IO04          0x51e
-           MX93_PAD_SD2_DATA2__GPIO3_IO05          0x51e
-           MX93_PAD_SD2_DATA3__GPIO3_IO06          0x51e
-           MX93_PAD_SD2_VSELECT__GPIO3_IO19        0x51e
-       >;
-   };
-
    /* need to config the SION for data and cmd pad, refer to ERR052021 */
    pinctrl_usdhc3: usdhc3grp {
        fsl,pins = <

The driver also needs the following rework.

--- a/drivers/net/ethernet/freescale/fec_ptp.c
+++ b/drivers/net/ethernet/freescale/fec_ptp.c
@@ -184,7 +184,8 @@ static int fec_ptp_enable_pps(struct fec_enet_private *fep, uint enable)
        val |= (1 << FEC_T_TF_OFFSET | 1 << FEC_T_TIE_OFFSET);
        val &= ~(1 << FEC_T_TDRE_OFFSET);
        val &= ~(FEC_T_TMODE_MASK);
-       val |= (FEC_HIGH_PULSE << FEC_T_TMODE_OFFSET);
+       // val |= (FEC_HIGH_PULSE << FEC_T_TMODE_OFFSET);
+       val |= (FEC_TMODE_TOGGLE << FEC_T_TMODE_OFFSET);
        writel(val, fep->hwp + FEC_TCSR(fep->pps_channel));

        /* Write the second compare event timestamp and calculate

After booting the board, run these commands:

$ ptp4l -A -4 -H -m -i eth0 &
$ echo 1 > /sys/class/ptp/ptp0/pps_enable

These will get the SD2_DATA0 or TP1009 running a square wave at 0.5 Hz through setting the ptp0 port with:

-A    Select the delay mechanism automatically. Start with E2E and switch to P2P when a peer delay request is received.

-4    Select the UDP IPv4 network transport. This is the default transport.

-H    Select the hardware time stamping.

-m    Print messages to the standard output.

JosephAtNXP_0-1725312576333.bmp

Run the next command to set the pps (1 Hz signal):

$ echo "0 $(date +%s) 100000000 1 0" > /sys/class/ptp/ptp0/period

The last because the current driver needs the actual date and a future start; in this case the signal will start within 100 ms, in order to work. You can try with different start times until the optimal value is found. [3]

JosephAtNXP_1-1725312604309.bmp

 

Hands-on for EQOS or eth1 MAC

This is reduced to the proper devicetree changes, and it does not have driver rework nor pps_enable control file.

It uses SD2_CLK or TP1008, so DTS need this adjustment:

--- imx93-11x11-evk.dts 2024-08-23 18:19:56.344798901 +0200
+++ imx93-11x11-evk-pps.dts     2024-09-02 21:31:46.569477421 +0200
@@ -100,18 +100,6 @@
        regulator-max-microvolt = <1800000>;
    };
 
-   reg_usdhc2_vmmc: regulator-usdhc2 {
-       compatible = "regulator-fixed";
-       pinctrl-names = "default";
-       pinctrl-0 = <&pinctrl_reg_usdhc2_vmmc>;
-       regulator-name = "VSD_3V3";
-       regulator-min-microvolt = <3300000>;
-       regulator-max-microvolt = <3300000>;
-       gpio = <&gpio3 7 GPIO_ACTIVE_HIGH>;
-       off-on-delay-us = <12000>;
-       enable-active-high;
-   };
-
    reg_vdd_12v: regulator-vdd-12v {
        compatible = "regulator-fixed";
        regulator-name = "reg_vdd_12v";
@@ -770,21 +766,6 @@
    status = "okay";
 };
 
-&usdhc2 {
-   pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep";
-   pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>;
-   pinctrl-1 = <&pinctrl_usdhc2_100mhz>, <&pinctrl_usdhc2_gpio>;
-   pinctrl-2 = <&pinctrl_usdhc2_200mhz>, <&pinctrl_usdhc2_gpio>;
-   pinctrl-3 = <&pinctrl_usdhc2_sleep>, <&pinctrl_usdhc2_gpio_sleep>;
-   cd-gpios = <&gpio3 00 GPIO_ACTIVE_LOW>;
-   fsl,cd-gpio-wakeup-disable;
-   vmmc-supply = <&reg_usdhc2_vmmc>;
-   bus-width = <4>;
-   status = "okay";
-   no-sdio;
-   no-mmc;
-};
-
&usdhc3 {
    pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep";
    pinctrl-0 = <&pinctrl_usdhc3>, <&pinctrl_usdhc3_wlan>;
@@ -822,14 +802,15 @@
            MX93_PAD_ENET1_RD1__ENET_QOS_RGMII_RD1                  0x57e
            MX93_PAD_ENET1_RD2__ENET_QOS_RGMII_RD2                  0x57e
            MX93_PAD_ENET1_RD3__ENET_QOS_RGMII_RD3                  0x57e
            MX93_PAD_ENET1_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK  0x58e
            MX93_PAD_ENET1_RX_CTL__ENET_QOS_RGMII_RX_CTL            0x57e
            MX93_PAD_ENET1_TD0__ENET_QOS_RGMII_TD0                  0x57e
            MX93_PAD_ENET1_TD1__ENET_QOS_RGMII_TD1                  0x57e
            MX93_PAD_ENET1_TD2__ENET_QOS_RGMII_TD2                  0x57e
            MX93_PAD_ENET1_TD3__ENET_QOS_RGMII_TD3                  0x57e
            MX93_PAD_ENET1_TXC__CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK  0x58e
            MX93_PAD_ENET1_TX_CTL__ENET_QOS_RGMII_TX_CTL            0x57e
+           MX93_PAD_SD2_CLK__ENET_QOS_1588_EVENT0_OUT              0x31e
        >;
    };

@@ -849,6 +830,7 @@
            MX93_PAD_ENET1_TD3__GPIO4_IO02                          0x31e
            MX93_PAD_ENET1_TXC__GPIO4_IO07                          0x31e
            MX93_PAD_ENET1_TX_CTL__GPIO4_IO06                       0x31e
+           MX93_PAD_SD2_CLK__GPIO3_IO01                            0x31e
        >;
    };

@@ -998,75 +982,6 @@
        >;
    };

-   pinctrl_reg_usdhc2_vmmc: regusdhc2vmmcgrp {
-       fsl,pins = <
-           MX93_PAD_SD2_RESET_B__GPIO3_IO07        0x31e
-       >;
-   };
-
-   pinctrl_usdhc2_gpio: usdhc2gpiogrp {
-       fsl,pins = <
-           MX93_PAD_SD2_CD_B__GPIO3_IO00           0x31e
-       >;
-   };
-
-   pinctrl_usdhc2_gpio_sleep: usdhc2gpiogrpsleep {
-       fsl,pins = <
-           MX93_PAD_SD2_CD_B__GPIO3_IO00           0x51e
-       >;
-   };
-
-   /* need to config the SION for data and cmd pad, refer to ERR052021 */
-   pinctrl_usdhc2: usdhc2grp {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__USDHC2_CLK            0x1582
-           MX93_PAD_SD2_CMD__USDHC2_CMD            0x40001382
-           MX93_PAD_SD2_DATA0__USDHC2_DATA0        0x40001382
-           MX93_PAD_SD2_DATA1__USDHC2_DATA1        0x40001382
-           MX93_PAD_SD2_DATA2__USDHC2_DATA2        0x40001382
-           MX93_PAD_SD2_DATA3__USDHC2_DATA3        0x40001382
-           MX93_PAD_SD2_VSELECT__USDHC2_VSELECT    0x51e
-       >;
-   };
-
-   /* need to config the SION for data and cmd pad, refer to ERR052021 */
-   pinctrl_usdhc2_100mhz: usdhc2-100mhzgrp {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__USDHC2_CLK            0x158e
-           MX93_PAD_SD2_CMD__USDHC2_CMD            0x4000138e
-           MX93_PAD_SD2_DATA0__USDHC2_DATA0        0x4000138e
-           MX93_PAD_SD2_DATA1__USDHC2_DATA1        0x4000138e
-           MX93_PAD_SD2_DATA2__USDHC2_DATA2        0x4000138e
-           MX93_PAD_SD2_DATA3__USDHC2_DATA3        0x4000138e
-           MX93_PAD_SD2_VSELECT__USDHC2_VSELECT    0x51e
-       >;
-   };
-
-   /* need to config the SION for data and cmd pad, refer to ERR052021 */
-   pinctrl_usdhc2_200mhz: usdhc2-200mhzgrp {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__USDHC2_CLK            0x15fe
-           MX93_PAD_SD2_CMD__USDHC2_CMD            0x400013fe
-           MX93_PAD_SD2_DATA0__USDHC2_DATA0        0x400013fe
-           MX93_PAD_SD2_DATA1__USDHC2_DATA1        0x400013fe
-           MX93_PAD_SD2_DATA2__USDHC2_DATA2        0x400013fe
-           MX93_PAD_SD2_DATA3__USDHC2_DATA3        0x400013fe
-           MX93_PAD_SD2_VSELECT__USDHC2_VSELECT    0x51e
-       >;
-   };
-
-   pinctrl_usdhc2_sleep: usdhc2grpsleep {
-       fsl,pins = <
-           MX93_PAD_SD2_CLK__GPIO3_IO01            0x51e
-           MX93_PAD_SD2_CMD__GPIO3_IO02            0x51e
-           MX93_PAD_SD2_DATA0__GPIO3_IO03          0x51e
-           MX93_PAD_SD2_DATA1__GPIO3_IO04          0x51e
-           MX93_PAD_SD2_DATA2__GPIO3_IO05          0x51e
-           MX93_PAD_SD2_DATA3__GPIO3_IO06          0x51e
-           MX93_PAD_SD2_VSELECT__GPIO3_IO19        0x51e
-       >;
-   };
-
    /* need to config the SION for data and cmd pad, refer to ERR052021 */
    pinctrl_usdhc3: usdhc3grp {
        fsl,pins = <

After boot, issue these commands:

$ ptp4l -A -4 -H -m -i eth1 &
$ echo "0 $(date +%s) 1000000000 1 0" > /sys/class/ptp/ptp1/period

You will have an squared wave of 1 Hz running within 1 s with the same settings as the FEC setup.

JosephAtNXP_2-1725312629341.bmp

 

Conclusion

Both PPS can run in the same image changes and DTS changes, proven in imx-linux-nanbield branch, with the manifest imx-6.6.3-1.0.0.xml.

And it's the start of testing IEEE 1588 and syncing capabilities of this i.MX 9 series processors.

Sources

[1] http://events17.linuxfoundation.org/sites/events/files/slides/elc_insop_2015.pdf

[2] https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-serials-IEEE1588-1pps-test-procedu...

[3] https://github.com/nxp-imx/linux-imx/blob/b586a521770e508d1d440ccb085c7696b9d6d387/Documentation/ABI...

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎09-06-2024 11:24 AM
更新者: