FRDM Device Trees for Education and Rapid Prototyping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM Device Trees for Education and Rapid Prototyping

FRDM Device Trees for Education and Rapid Prototyping

To simplify development on the NXP FRDM board family, new device trees have been created for the i.MX91, i.MX93, i.MX95, and i.MX8MP platforms. These device trees are intended to provide a more ready to use out of the box experience by preconfiguring the Raspberry Pi connector with the same peripheral mapping commonly expected on Raspberry Pi compatible hardware.

With this approach, developers, students, and makers can use compatible expansion boards and HAT style accessories more easily, without needing to create or significantly modify additional device tree files. Instead of spending time on low level hardware description updates, users can start evaluating peripherals and building applications directly on top of the provided configurations.


For convenience, this post includes a .zip package containing:

  • The compiled device tree binaries (.dtb)
  • The device tree source files (.dts)
  • The kernel patch for the NXP Linux Kernel 6.18 required to integrate these changes

All files are attached to this post, allowing users to easily reuse, modify, or integrate the device trees into their own projects.

To configure a new device tree, compile it, and flash it onto the target, you can refer to the following guides:

How to compile Linux Kernel Image and device tree using Yocto SDK
Flash customized Linux Kernel Image and device tree using UUU Tool

添付
評価なし
バージョン履歴
最終更新日:
‎06-04-2026 08:12 AM
更新者: