Config Tools for i.MX v25.06 Now Available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config Tools for i.MX v25.06 Now Available

Config Tools for i.MX v25.06 Now Available

We are pleased to announce that Config Tools for i.MX v25.06 are now available.

Downloads & links

Release Notes

Full details on the release (features, known issues...)

• DDR
– Support for i.MX 91 is added.
– Synchronized with BSP Q2 release
– Support for the i.MX 91 FRDM board is added.
– Support for the i.MX 93 FRDM board is added.
– Spectrum support for i.MX 95 and i.MX 943 is spread.
– The Address mirroring option in the UI for all mscale devices with DDR3L and DDR4 is exposed.
– DDR3L support for i.MX 8M and i.MX 8MM is added.
– Linux support for code generation (beta) is added.
• SerDes tool
– i.MX 943 support (Beta) is added.
• Clocks
– Support for read-only element settings is added.
– Filtering all settings of Initialization modules in the Details view is supported.
• Peripherals
– A wizard to export the Registers view data in the CSV format is supported.
– Performance of the tool is improved.
• An ability to export/import Expansion Boards and Expansion Headers is added.

No ratings
Version history
Last update:
‎07-03-2025 06:44 AM
Updated by: