lunarG sdk is broken so the NXP framework is not useable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lunarG sdk is broken so the NXP framework is not useable

848 Views
foxsquirrel
Contributor II

We use Ubuntu 22.04 and the lunarG sdk has some issues and will not install so the NXP framework will not work either. Looked it over and tried to grab this and that and try to make it work but that did not work out. My question is what do we do at this point, any suggestions on this.

0 Kudos
Reply
2 Replies

829 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Which board are you using? since the Mx8 works nicelly but with yocto, you can download the BSP from:

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

 

Regards

0 Kudos
Reply

826 Views
foxsquirrel
Contributor II

Hi,

We are using Variscite imx8m, imx93, 6ul.

I am using the Varsicte BSP (yocto), was under the assumption it was NXP with some tweaks.

Problem we are having is launching Vulkan and Opengles2.

No problems with Gtk3. Fltk has an issue with the mouse. Touchscreen works fine with Fltk, the cursor disappears when it is in the Fltk screen.

Need to create some application specific graphics and wanted to go with straight wayland and Vulkan.

 

Thank you for the link, was not aware of that information until now.

 

Regards,

Fred

0 Kudos
Reply