i.MX8MM DRM framebuffer does not show splash/logo image during or after kernel boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8MM DRM framebuffer does not show splash/logo image during or after kernel boot

1,146 次查看
hyilmaz
Contributor I

Hello,

I'm working on an i.MX8M Mini (i.MX8MM) based board and I'm trying to display a splash screen or any image (even test pattern or static logo) using framebuffer (fb) or DRM/KMS during early boot (kernel stage or just after).

  • U-Boot splash/logo is working fine and shown on display.

  • When the kernel boots, the display turns black (screen resets).

  • dmesg shows that imx-drm and fb0 are initialized correctly:

  • /dev/fb0 exists, but writing to it (using tools like fbv, cat, or custom code) does not result in anything on the screen.

  • Weston works correctly when launched later from the rootfs — it enables the display and rendering works as expected.

    What I've Checked:

    • Kernel has CONFIG_DRM, CONFIG_DRM_IMX, CONFIG_DRM_FBDEV_EMULATION, etc. enabled.

    • Device Tree has proper lcdif, mipi_dsi, and panel nodes.

    • Weston runs with drm-backend.so and works well, so the display pipeline is functional.

    What I want to achieve:

    I want to:

    • Show a splash screen during or just after kernel boot (before Weston starts).

    • Possibly write raw image data directly to framebuffer or use fbv, psplash, or something similar.

    Questions:

    1. Is there anything specific I should enable in the DRM or IMX DRM driver to get early framebuffer working?

    2. Is there a known limitation on imx-drm not supporting fbdev write access until userspace enables the pipeline?

    3. Is there an example of using fb0 directly on i.MX8MM DRM to display a raw image without Weston?

    Thank you in advance.

0 项奖励
回复
1 回复

1,129 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @hyilmaz 

There are some reference solutions for continuous display of logos, please create a SFDC case so that we can share such solutions.

Best Regards,
Zhiming

0 项奖励
回复