i.MX6 Color Correction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Color Correction

1,685件の閲覧回数
steffendoster
Contributor IV

Hi everyone,

currently I'm working on a custom i.MX6DL Board wih Mainline Linux-Kernel.
But the display attached to it does need some color-correctien (red seems more like orange).
The Display is a small RGB-Display, so no LDB is used.

I know that the IPU is capable of doing that, but it seems, that the Mainline-Kernel doesn't support it. So I want to switch to the Community-Kernel, but I'm having some problems.
I managed to boot the Community-Kernel, but it doesn't show anything on the display.

Also it's lacking the /dev/fb* Devices and /dev/dri/card1

I checked it on SabreSD, too. Mainline Kernel shows Tux and a Command-Line via HDMI, Community-Kernel doesn't, although there are four /dev/fb* (but also no /dev/dri/card1).

I know it must be a Devicetree-Issue, but I'm not sure where to get the right hints for this.

Are there any Devicetree snippets available out there?
Do you need more details?

Greetings
Steffen

 

0 件の賞賛
返信
0 返答(返信)