While checking the BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

While checking the BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs

跳至解决方案
2,604 次查看
jj0371
Contributor I

Hi I am testing FRDM33772BSPIEVB and S32K144EVB-Q100. While checking the BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs. The battery pack is not connected. Is there a way to check the code normally without the battery pack?

标签 (1)
0 项奖励
回复
1 解答
2,470 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jang,

 

The connection of a battery pack is not strictly required for getting the mentioned example working. However, the battery pack connector is used also for supplying the MC33772B device itself. Therefore, you should use at least pins X1-2 (POS_BATT) and X1-34 (NEG_BATT) of the battery pack connector to supply the device, e.g. by 12V.

 

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,471 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jang,

 

The connection of a battery pack is not strictly required for getting the mentioned example working. However, the battery pack connector is used also for supplying the MC33772B device itself. Therefore, you should use at least pins X1-2 (POS_BATT) and X1-34 (NEG_BATT) of the battery pack connector to supply the device, e.g. by 12V.

 

Best regards,

Tomas

0 项奖励
回复