コミュニティを検索
01-23-2026
12:02 PM
1件の賞賛
This patch series enables the external 3.3 V and 5 V power rails used by the Raspberry Pi expansion connector on the i.MX93-QSB, i.MX93-FRDM, and i.MX91-FRDM boards. These regulators were a...
12-29-2023
09:58 AM
Hi Everyone, I am trying to understand the power management architecture on i.MX9 series. Where I am coming from is, we know Power is managed by PMICs. Since initial days only way to regulate p...
05-03-2025
10:14 PM
From RM00294 i.MX VPU Application Programming Interface Linux Reference Manual: "... Besides the VPU wrapper API (deprecated), the V4L2-based framework on top of the user library is d...
01-19-2024
06:35 AM
Can i.MX9 work with only 24MHz clock if no low power/stand-by mode is needed and an external RTC is present?
01-28-2026
01:31 AM
Hi, Thanks! I want to integrate TPM2.0 with i.MX9 processor (using custom board). Requirement is to boot i.MX9 with Yocto 5.0 Linux image including TPM2.0 support which should enable secure/t...
04-14-2025
07:59 PM
Hi All, we are working to test the secure boot feature on i.MX9 series namely i.MX95 and i.MX93. we are searching relevant documentation (Application notes) for the same. But we yet to find i...
01-19-2024
03:47 AM
Hi iMX Champ My customer would like to use Android OS with i.MX93 series. Can you please check if i.MX 9 series can be supported with imx-android sdk? Thanks and Regards, Jack
07-20-2026
01:58 AM
Can the provisioned certificate and private key on the i.MX93 be used directly to establish HTTPS/TLS connections? If yes, what is the recommended method for accessing and utilizing these c...
11-27-2024
01:52 AM
There will be a setup of the iMX9 with Linux on the A55 cores and FreeRTOS on the M33 core. I currently do initial stuff on the M33. Question 1: for a magnetic pickup sensor (frequency sensor) I n...