コミュニティを検索
10-22-2025
01:25 AM
Hi,
Infineon engineers have successfully enabled SEMPER™ (S28HS512T) and HYPERFLASH™ (S26KS256S) flash memory on the S32G SoC and shared their Application Notes with us.
The documentation m...
ラベル:
04-21-2023
02:32 AM
2件の賞賛
...源的初始化,解决M核和A核的资源冲突,并且启动M和A核。所以理论上运行M PFE Master Mcal驱动加A PFE Slave Linux驱动也是需要一个bootloader的。参考文档《S32G_Bootloader_V*》,Johnli,可以在公开community上搜索获得。
本文讨论一种简易的办法,就是:
S32G3 RDB3板子配置为SDcard启动,插入S...
- タグ:
- 1
ラベル:
09-09-2022
12:41 AM
2件の賞賛
This doc explain how to modify the bootloader to boot linux&mcal, to solve the conflict between bootloader, mcal and linux
本文说明在S32G2 RDB2板上如何定制开发Bootloader,本文示例主要实现功能是:
B...
ラベル:
コメントの結果を表示(5)
-
Hi @Johnli 您好! 在ATF中,部分时钟为什么没有定义具体的时钟值,如下图红框中。像这种时钟,系统如何确定...
-
Hi @Johnli 您好!非常感谢~ 再请教您个问题。我在您分享文档中以及EB中,经常看到 "Under MCU ...
-
Hi @Johnli, 您好! 目前正在使用S32,您发布的文档对我帮助很大,非常感谢! 请教您个...
-
...ogger demo https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-G3-Customization/t...
-
check the doc: make sure you have load the llce driver ko. S32G...
11-30-2025
07:50 AM
...ay be assigned to different Ethernet ports by the DHCP server connected to each port on the S32G-VNP-RDB3 board.
This default behavior is convenient for most customers, as it requires no additional n...
ラベル:
02-10-2026
12:17 AM
本文说明如何检查S32DS Flash Tool的默认波特率,以便确认下载相关的失败问题,以及如何解决。
目录
1 背景与资料说明... 2
1.1 背景说明... 2
1.2 所需资料说明... 4
2 S32G波特率设置说明... 4
3 &n...
ラベル:
01-16-2022
09:56 PM
This doc expain how to use eMMC from user space, contents as follows:
目录 1 eMMC的分区情况 ...................................................... 2 2 S32G+BSP29上默认的eMMC启动 ............................ 3...
ラベル:
01-16-2022
09:38 PM
1件の賞賛
This doc explain where is the design resource and what they are of S32G in Chinese, Contents as follows:
目录 1 www.nxp.com 官网资源 ............................................. 2 1.1...
ラベル:
01-16-2022
09:54 PM
2件の賞賛
This doc explain our Linux BSP driver and how to custom them. Contests as follows: include bsp30/32
目录 1 S32G Linux文档说明 ................................................. 2 2 创建S32G RDB2 Linux板级开发...
ラベル:
4 週間前
Hi NXP: I would like to know if S32G399 supports the independent reset of a specific M7 core without affecting the normal operation of other cores?