コミュニティを検索
07-27-2025
07:24 PM
...bstract
This document is intended to guide developers to integrate the EdgeLock® SE050 security chip on the NXP FRDM-i.MX91 development board to achieve hardware-level security enhancement....
1ヶ月前
...bstract
This document is intended to guide developers to integrate the EdgeLock® SE050 security chip on the NXP MIMXRT1180EVK development board to achieve hardware-l...
04-08-2021
11:22 AM
You need to get a lot of things right to build a truly secure system. Join this session to learn how the EdgeLock™ secure enclave that’s built into our i.MX 8ULP applications processors protects t...
06-10-2025
08:12 AM
Hello NXP community, I am using SE051 with embedded Linux, where I store private key in SE051 and certificate is in file system, embedded Linux board run as TLS server and want to enable mutual auth...
ラベル
- ラベル:
-
SE050
01-09-2025
10:23 AM
I'm new to the EdgeLock Secure Enclave ("ELE" in the KW45 reference manual) and I have several questions I couldn't find answers in various NXP resources online: 1) Where can I find more d...
04-09-2021
02:10 PM
The EdgeLock™ SE050 family provides a root of trust at the IC level. This CC EAL6+ certified secure element also supports compliance to standards such as ISO/IEC 62443 SL3. The EdgeLock SE050 s...
06-25-2025
10:37 AM
I would like to use Zephyr's open source MCUBoot module on an IoT project using the FRDM-MCXN947 board, but also use the Edgelock Secure Enclave to increase key security. Am I correct that this w...
06-25-2024
10:41 PM
Dear community, We are currently implementing secure element based security for our PX4-based drone firmware. The pixhawk hardware supports SE050 + Kinetis K66_180 MPU. We have already explored the ...
07-10-2020
05:02 AM
1件の賞賛
This example shows all steps for an onboarding process of a device to AWS IoT Core using the pre-provisioned credentials of the EdgeLock SE050E secure element.
AWS IoT authenticates client c...
ラベル:
03-12-2020
07:25 AM
1件の賞賛