Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
7,000 results
Sorted by:
01-22-2024
11:55 PM
NXP offers FW update code as part of the SW6705.
PN7160 is typically delivered with the initial FW 12.50.05. To ensure full reliable functionality, it is highly recommend...
Labels:
09-23-2021
08:14 PM
1 Kudo
RT600 MCUXpresso JLINK debug QSPI flash
1 Introduction
MIMXRT600-EVK is the NXP official board, which onboard flash is the external octal flash, the octal flash is connected t...
Labels:
03-14-2024
01:57 AM
Goodday, I'm on MCUXpresso IDE v11.9.0 [Build 2144] and have JN5189DK6 V2.6.13 installed. In the Application Notes AN1244 in Section 8.2 is descripted how to change the Touchlink P...
Labels
- Labels:
-
Product: JN518X
07-31-2023
01:24 PM
Hi, Im having troubles trying to load an SDK to MCUxpresso IDE, i download them from the SDK builder from NXP and i make them only for MCUxpresso IDE. But it continues to show me the error that the S...
01-09-2024
08:46 AM
Hi, I'm trying to setup a timer in MCUXPresso with lpc804 mcu. I have configured the timer as below. How can I define a callback to trigger on timer?
Labels
- Labels:
-
LPC800
07-27-2021
08:39 PM
1 Kudo
Recently I found some customers have a bit of problem when porting project from one MCU to another, so this article using simple steps demonstrates how to change MCU with MCUXpresso. There is also a...
2 weeks ago
In the MCUXpresso IDE, is there a way to draw in a window a data series ? For example draw the content of an array graphically. Luigi
4 weeks ago
I have previously used the TWR-K60D100M board to run the HVAC demo application with MQX/Codewarrior. We are migrating to MCUxpresso and FreeRTOS for our new product development platforms. Is there a...
Show results in replies (3)
-
...et familiar with MCUXpresso-IDE you can consult its respective page where you will found trainings a...
-
...o HVAC demo for K60 with MCUXpresso. However there is a HVAC solution with MagniV: Designing S...
-
...ame processor for the new design but develop the application with the MCUxpresso FreeRTOS tools. T...
11-24-2016
04:03 PM
This documents describes how to use this tool in order to generate the routing and muxing for pins. This tool is available as an online WEB application https://mcuxpresso.nxp.com Pins Tool O...