imx8mqevk -camera pyeiq issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mqevk -camera pyeiq issues

2,271 Views
manizillion
Contributor IV

Hi ,

I am using imx8mqevk and camera SCH -29653 REV A1 Mipi csi on molex connectors connected.

On the latest 5.4 build i see the static image apps for pyeiq is ok, but when it comes to live camera the face detection or the object detection application is not working at all, response is very slow ..

Please validate if my camera module is ok ?

Regards
Mani

Labels (1)
Tags (1)
0 Kudos
1 Reply

2,250 Views
manish_bajaj
NXP Employee
NXP Employee

[email protected]‌,

Quick note, PYeIQ provide easy demo platform and we expect anyone to use it for reference.

8MQ EVK doesnot have molex connectors, so do you have your own adapter board to convert Molex to SaS connector?

-manish

0 Kudos