i.MX RT Camera Capture for Model Training

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT Camera Capture for Model Training

i.MX RT Camera Capture for Model Training

The attached project enables users to capture and save the camera data captured by a i.MXRT1060-EVK board onto a microSD card.

This project does not do inferencing of a model. Instead it is meant to be used to generate images that can then be used on a PC for training a model. The images are saved in RGB NHWC format as a binary file on the microSD card, and then a Python script running on the PC can convert those binary files into the PNG image format.

 

Software requirements
====================
- MCUXpresso IDE 11.2.x
- MCUXpresso SDK for RT1060

Hardware requirements
=====================
- Micro USB cable
- IMXRT1060-EVK board with included camera + RK043FN02H-CT LCD
- MicroSD card
- Personal computer (Windows)
- Micro SD card reader
- Python 3.x installed

Board settings
==============
Camera and LCD connected to i.MXRT1060-EVK

Prepare the demo
================
1. Insert a micro SD card into the micro SD card slot on the i.MXRT1060-EVK (J39)

2. Open MCUXpresso IDE 11.2 and import the project using "Import project(s) from file system.." from the Quickstart panel. Use the "Archive" option to select the zip file that contains this project.

3. If desired, two #define values can be modified in camera_capture.c to adjust the captured image size:
#define EXTRACT_HEIGHT 256 //Max EXTRACT_HEIGHT value possible is 271 (due to border drawing)
#define EXTRACT_WIDTH 256 //Max EXTRACT_WIDTH value possible is 480

4. Build the project by clicking on "Build" in the Quickstart Panel

5. Connect a USB cable between the host PC and the OpenSDA port (J41) on the target board.

6. Open a serial terminal with the following settings:
- 115200 baud rate
- 8 data bits
- No parity
- One stop bit
- No flow control

7. Download the program to the target board by clicking on "Debug" in the Quickstart Panel

8. Click on the "Resume" icon to begin running the demo.

Running the demo
================
The terminal will ask for a classification name. This will create a new directory on the SD card with that name. The name size is limited to 5 characters because the FATFS file system supports only 8 characters in a file name, and three of those characters are used to number the images.

For best results, the selection rectangle should be centered on the image and nearly (but not completely)  fill up the whole rectangle. The camera should be stabilized with your finger or by some other means to prevent shaking. Also ensure the camera lens has been focused as described in the instructions when connecting the camera and LCD.


While running the demo, press the 'c' key to enter a new classification name, or press 'q' to quit the program and remove the micro SD card.

Transfer the .bin files created on the SD card to your PC in the same directory that the Python script which can be found in the "scripts" directory to convert the images to PNG format.

If the captured image is a square (width==height) the script can be called with:
python convert_image.py directory_name
which will convert all the .BIN files in the specified directory name to PNG files.

If the captured image is not a square, the width and height can be specified at the command line:
python convert_image.py directory_name width height


Terminal Output
==============
Camera SD Card Capture
Extracted Image: Height x Width: 256x256

Please insert a card into board.

Card inserted.
Mounting SD Card

Enter name of new class (must be less than 5 characters):
test

Creating directory test......

Press any key to capture image. Press 'c' to change class or 'q' to quit

Writing file /test/test001.bin......
Write Complete
Press any key to capture image. Press 'c' to change class or 'q' to quit

Remove SD Card

Labels (1)
Attachments
%3CLINGO-SUB%20id%3D%22lingo-sub-1168450%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3Ei.MX%20RT%20Camera%20Capture%20for%20Model%20Training%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1168450%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%0A%3CP%3EThe%20attached%20project%20enables%20users%20to%20capture%20and%20save%20the%20camera%20data%20captured%20by%20a%20i.MXRT1060-EVK%20board%20onto%20a%20microSD%20card.%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3EThis%20project%20does%20not%20do%20inferencing%20of%20a%20model%3C%2FSTRONG%3E.%20Instead%20it%20is%20meant%20to%20be%20used%20to%20generate%20images%20that%20can%20then%20be%20used%20on%20a%20PC%20for%20training%20a%20model.%20The%20images%20are%20saved%20in%20RGB%20NHWC%20format%20as%20a%20binary%20file%20on%20the%20microSD%20card%2C%20and%20then%20a%20Python%20script%20running%20on%20the%20PC%20can%20convert%20those%20binary%20files%20into%20the%20PNG%20image%20format.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3ESoftware%20requirements%3C%2FSTRONG%3E%3CBR%20%2F%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3CBR%20%2F%3E-%3CSPAN%3E%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Fmcuxpresso-software-and-tools-%2Fmcuxpresso-integrated-development-environment-ide%3AMCUXpresso-IDE%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EMCUXpresso%20IDE%2011.2.x%3C%2FA%3E%3CBR%20%2F%3E-%3CSPAN%3E%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fmcuxpresso.nxp.com%2Fen%2Fselect%3Fdevice%3DEVK-MIMXRT1060%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EMCUXpresso%20SDK%20for%20RT1060%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3EHardware%20requirements%3C%2FSTRONG%3E%3CBR%20%2F%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3CBR%20%2F%3E-%20Micro%20USB%20cable%3CBR%20%2F%3E-%3CSPAN%3E%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdevelopment-boards%2Fi-mx-evaluation-and-development-boards%2Fmimxrt1060-evk-i-mx-rt1060-evaluation-kit%3AMIMXRT1060-EVK%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EIMXRT1060-EVK%20board%3C%2FA%3E%3CSPAN%3E%26nbsp%3B%3C%2FSPAN%3Ewith%20included%20camera%20%2B%3CSPAN%3E%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fpart%2FRK043FN02H-CT%23%2F%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3ERK043FN02H-CT%20LCD%3C%2FA%3E%3CBR%20%2F%3E-%20MicroSD%20card%3CBR%20%2F%3E-%20Personal%20computer%20(Windows)%3CBR%20%2F%3E-%20Micro%20SD%20card%20reader%3CBR%20%2F%3E-%20Python%203.x%20installed%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3EBoard%20settings%3C%2FSTRONG%3E%3CBR%20%2F%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3CBR%20%2F%3E%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fi-MX-RT-Knowledge-Base%2FConnecting-camera-and-LCD-to-i-MX-RT-EVKs%2Ftac-p%2F1122184%22%20target%3D%22_self%22%3ECamera%20and%20LCD%20connected%20to%20i.MXRT1060-EVK%3C%2FA%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3EPrepare%20the%20demo%3C%2FSTRONG%3E%3CBR%20%2F%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3CBR%20%2F%3E1.%20Insert%20a%20micro%20SD%20card%20into%20the%20micro%20SD%20card%20slot%20on%20the%20i.MXRT1060-EVK%20(J39)%3C%2FP%3E%0A%3CP%3E2.%20Open%20MCUXpresso%20IDE%2011.2%20and%20import%20the%20project%20using%20%22Import%20project(s)%20from%20file%20system..%22%20from%20the%26nbsp%3BQuickstart%20panel.%20Use%20the%20%22Archive%22%20option%20to%20select%20the%20zip%20file%20that%20contains%20this%20project.%3C%2FP%3E%0A%3CP%3E3.%20If%20desired%2C%20two%20%23define%20values%20can%20be%20modified%20in%20camera_capture.c%20to%20adjust%20the%20captured%20image%20size%3A%3CBR%20%2F%3E%23define%20EXTRACT_HEIGHT%20256%20%2F%2FMax%20EXTRACT_HEIGHT%20value%20possible%20is%20271%20(due%20to%20border%20drawing)%3CBR%20%2F%3E%23define%20EXTRACT_WIDTH%20256%20%2F%2FMax%20EXTRACT_WIDTH%20value%20possible%20is%20480%3C%2FP%3E%0A%3CP%3E4.%20Build%20the%20project%20by%20clicking%20on%20%22Build%22%20in%20the%20Quickstart%20Panel%3C%2FP%3E%0A%3CP%3E5.%20Connect%20a%20USB%20cable%20between%20the%20host%20PC%20and%20the%20OpenSDA%20port%20(J41)%20on%20the%20target%20board.%3C%2FP%3E%0A%3CP%3E6.%20Open%20a%20serial%20terminal%20with%20the%20following%20settings%3A%3CBR%20%2F%3E-%20115200%20baud%20rate%3CBR%20%2F%3E-%208%20data%20bits%3CBR%20%2F%3E-%20No%20parity%3CBR%20%2F%3E-%20One%20stop%20bit%3CBR%20%2F%3E-%20No%20flow%20control%3C%2FP%3E%0A%3CP%3E7.%20Download%20the%20program%20to%20the%20target%20board%20by%20clicking%20on%20%3CSTRONG%3E%22Debug%22%3C%2FSTRONG%3E%20in%20the%20Quickstart%20Panel%3C%2FP%3E%0A%3CP%3E8.%20Click%20on%20the%20%3CSTRONG%3E%22Resume%22%3C%2FSTRONG%3E%20icon%20to%20begin%20running%20the%20demo.%3C%2FP%3E%0A%3CP%3ERunning%20the%20demo%3CBR%20%2F%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3CBR%20%2F%3EThe%20terminal%20will%20ask%20for%20a%20classification%20name.%20This%20will%20create%20a%20new%20directory%20on%20the%20SD%20card%20with%20that%20name.%20The%20name%20size%20is%20limited%20to%205%20characters%20because%20the%20FATFS%20file%20system%20supports%20only%208%26nbsp%3Bcharacters%20in%20a%20file%20name%2C%20and%20three%20of%20those%20characters%20are%20used%20to%20number%20the%20images.%3C%2FP%3E%0A%3CP%3EFor%20best%20results%2C%20the%20selection%20rectangle%20should%20be%20centered%20on%20the%20image%20and%20nearly%20(but%20not%20completely)%26nbsp%3B%20fill%20up%20the%20whole%20rectangle.%20The%20camera%20should%20be%20stabilized%20with%20your%20finger%20or%20by%20some%20other%20means%20to%20prevent%20shaking.%20Also%20ensure%20the%20camera%20lens%20has%20been%20focused%20as%20described%20in%20the%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fi-MX-RT-Knowledge-Base%2FConnecting-camera-and-LCD-to-i-MX-RT-EVKs%2Ftac-p%2F1122184%22%20target%3D%22_self%22%3Einstructions%20when%20connecting%20the%20camera%20and%20LCD.%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E%3CBR%20%2F%3EWhile%20running%20the%20demo%2C%20press%20the%20'c'%20key%20to%20enter%20a%20new%20classification%20name%2C%20or%20press%20'q'%20to%20quit%20the%20program%20and%20remove%20the%20micro%20SD%20card.%3C%2FP%3E%0A%3CP%3ETransfer%20the%20.bin%20files%20created%20on%20the%20SD%20card%20to%20your%20PC%20in%20the%20same%20directory%20that%20the%20Python%20script%20which%20can%20be%20found%20in%20the%20%3CSTRONG%3E%22scripts%22%3C%2FSTRONG%3E%20directory%20to%20convert%20the%20images%20to%20PNG%20format.%3C%2FP%3E%0A%3CP%3EIf%20the%20captured%20image%20is%20a%20square%20(width%3D%3Dheight)%20the%20script%20can%20be%20called%20with%3A%3CBR%20%2F%3E%3CSTRONG%3Epython%20convert_image.py%20directory_name%3C%2FSTRONG%3E%3CBR%20%2F%3Ewhich%20will%20convert%20all%20the%20.BIN%20files%20in%20the%20specified%20directory%20name%20to%20PNG%20files.%3C%2FP%3E%0A%3CP%3EIf%20the%20captured%20image%20is%20not%20a%20square%2C%20the%20width%20and%20height%20can%20be%20specified%20at%20the%20command%20line%3A%3CBR%20%2F%3E%3CSTRONG%3Epython%20convert_image.py%20directory_name%20width%20height%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CBR%20%2F%3E%3CSTRONG%3ETerminal%20Output%3C%2FSTRONG%3E%3CBR%20%2F%3E%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3D%3CBR%20%2F%3ECamera%20SD%20Card%20Capture%3CBR%20%2F%3EExtracted%20Image%3A%20Height%20x%20Width%3A%20256x256%3C%2FP%3E%0A%3CP%3EPlease%20insert%20a%20card%20into%20board.%3C%2FP%3E%0A%3CP%3ECard%20inserted.%3CBR%20%2F%3EMounting%20SD%20Card%3C%2FP%3E%0A%3CP%3EEnter%20name%20of%20new%20class%20(must%20be%20less%20than%205%20characters)%3A%3CBR%20%2F%3Etest%3C%2FP%3E%0A%3CP%3ECreating%20directory%20test......%3C%2FP%3E%0A%3CP%3EPress%20any%20key%20to%20capture%20image.%20Press%20'c'%20to%20change%20class%20or%20'q'%20to%20quit%3C%2FP%3E%0A%3CP%3EWriting%20file%20%2Ftest%2Ftest001.bin......%3CBR%20%2F%3EWrite%20Complete%3CBR%20%2F%3EPress%20any%20key%20to%20capture%20image.%20Press%20'c'%20to%20change%20class%20or%20'q'%20to%20quit%3C%2FP%3E%0A%3CP%3ERemove%20SD%20Card%3C%2FP%3E%0A%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1168450%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3Ei.MX%20RT%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E
No ratings
Version history
Last update:
‎10-15-2020 03:12 PM
Updated by: