PRELU operation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PRELU operation error

2,479件の閲覧回数
dbinaghi
Contributor I

Hi,

I'm using a iMX8M Plus with a quantised tensorflow lite model (uint8).
The tflite 
runtime version is the 2.3.1.

My model contains some PRELU operations that according to the guide is a supported operation.

A warning is reported:

WARNING: Operator PRELU (v1) refused by NNAPI delegate: Input should be Float or UINT8

I think this is due to the fact that the tensor during processing becomes an int8 but it should be supported. This warning does not happen if I use a RELU activation function instead of PRELU.

The quantised model is attached.

Could you help me?
Thanks!  

 
0 件の賞賛
0 返答(返信)