NXP i.XM8MP EVK:reject TRANSPOSE, reject PAD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP i.XM8MP EVK:reject TRANSPOSE, reject PAD

1,904 Views
Geo
Contributor I

My Environment
Hardware: NXP i.XM8MP EVK A01
Software: Android version 10
insightface pytorch project link:https://github.com/deepinsight/insightface/tree/master/recognition/arcface_torch
pytorch pre-train model download link:https://onedrive.live.com/?cid=4a83b6b633b029cc&id=4A83B6B633B029CC%215577&authkey=!AFZjr283nwZHqbA


I use benchmark run this model resnet_r100_quant_2.5.0.tflite then output message as follows.

./android_aarch64_benchmark_model_plus_flex --num_threads=4 --graph=resnet_r100_quant_2.5.0.tflite --use_nnapi=true --enable_op_profiling=true > resnet_r100_quant_2.5.0.txt

05-16 19:18:43.179 I//vendor/bin/hw/[email protected]( 305): getSupportedOperations exit
05-16 19:18:43.181 I//vendor/bin/hw/[email protected]( 305): getSupportedOperations
05-16 19:18:43.181 I//vendor/bin/hw/[email protected]( 305): reject TRANSPOSE because >=4D or transposed on Batch not supported
05-16 19:18:43.181 I//vendor/bin/hw/[email protected]( 305): reject PAD because pad value for 3rd or 0rd/3rd dimensions
05-16 19:18:43.181 I//vendor/bin/hw/[email protected]( 305): reject TRANSPOSE because >=4D or transposed on Batch not supported
05-16 19:18:43.181 I//vendor/bin/hw/[email protected]( 305):
05-16 19:18:43.181 I//vendor/bin/hw/[email protected]( 305): getSupportedOperations exit
05-16 19:18:43.182 I//vendor/bin/hw/[email protected]( 305): getSupportedOperations
05-16 19:18:43.183 I//vendor/bin/hw/[email protected]( 305): reject TRANSPOSE because >=4D or transposed on Batch not supported
05-16 19:18:43.183 I//vendor/bin/hw/[email protected]( 305): reject TRANSPOSE because >=4D or transposed on Batch not supported


This model is downloaded from the insightface pytorch project.
Step 1:use the pytorch tool to convert pytorch to onnx (pytorch 1.7.1)
Step 2:use onnx-tf to convert onnx to pb. (onnx-tf 1.6.0)
Step 3:use TensorFlow to convert pb to tflite (resnet_r100_quant_2.5.0.tflite). (TensorFlow 2.5.0)


How to solve the issue as follows
reject TRANSPOSE because >=4D or transposed on Batch not supported
reject PAD because pad value for 3rd or 0rd/3rd dimensions

Attach file is the result of benchmark.

0 Kudos
0 Replies