Image Classification example of TF-lite do not use GPU on iWG27M iMX8QM kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Image Classification example of TF-lite do not use GPU on iWG27M iMX8QM kit

Jump to solution
4,345 Views
kushal_chaudhar
Contributor I

Hi

I tested  the Image classification example given in UM11226 section 7.2 On iWG27M iMX8QM SOM development kit, with Yocto ML manifest having 4.9.51 beta kernel with Opencl support.

It works fine and predicts the results in around 300 ms but it does not uses GPU. gputop application do not show any process running.

So My questions are

1) Why the application is not using GPU for its execution? (In spite of OpenCL support).

2) What needs to be done to use the GPU support.

3) I need TensorFlow-lite object detection example which utilize GPU for its execution, where Can I find that?

Labels (1)
0 Kudos
1 Solution
3,986 Views
vanessa_maegima
NXP Employee
NXP Employee

Hi [email protected]‌,

There's no GPU support on eIQ yet.

Thanks,

Vanessa

View solution in original post

0 Kudos
2 Replies
3,986 Views
simple_do
Contributor I

Hi Vanessa Maegima:

      there is example for tf-lite on  gpu run, it's avalible.

pastedImage_1.png

0 Kudos
3,987 Views
vanessa_maegima
NXP Employee
NXP Employee

Hi [email protected]‌,

There's no GPU support on eIQ yet.

Thanks,

Vanessa

0 Kudos