Can't use GPU to run TensorFlow DEMO on iMX8/8MP/8QM platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't use GPU to run TensorFlow DEMO on iMX8/8MP/8QM platform

2,590件の閲覧回数
weilly_li
Contributor IV

Hi,


There has some issue about Using TensorFlow DEMO on iMX8/8MP/8QM platform.

I tried run the binary of "label_image" as these instruction...
BSP : L5.10.35.2.0.0
(1) export USE_GPU_INFERNCE=1
(2) ./label_image -m mobilenet_v1_1.0_224_quant.tflite -l labels.txt -i dog.bmp -a 0
(3) ./label_image -m mobilenet_v1_1.0_224_quant.tflite -l labels.txt -i dog.bmp -a 1

weilly_li_0-1633666936141.png

 

the result show ... CPU and GPU inference time is same... seem GPU isn't running ?

and I found the warning of "W [query_hardware_caps:66]Unsupported evis version" while I using gpu.

So, have someone ever meet the same things ?
please help me... thank you

Weilly Li

0 件の賞賛
0 返答(返信)