Zephyr Zigbee support roadmap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zephyr Zigbee support roadmap

2,786 Views
jashka
Contributor I

Hello!
We are considering MCXW71 for a Zephyr project.

Zigbee is a key requirement but currently appears to only be supported through MCUXpresso.

1. Are there plans to add Zigbee support though Zephyr directly (i.e through KConfig)

2. Is the current alternative to generate Zigbee projects using MCUXpresso and then mix in Zephyr through CMake?

 

Best,

Jaagup

Tags (3)
0 Kudos
Reply
1 Reply

2,745 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

 

Currently we only have available for Zephyr the different features mentioned in the official documentation 

FRDM-MCXW71 — Zephyr Project Documentation 

 

To make use of some other feature or protocol of the device, you will need to go through the MCUXpresso IDE and the SDK releases

 

 Regards 

 

 

0 Kudos
Reply