Memory details with Zephyr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory details with Zephyr

Memory details with Zephyr

If you have any questions or issues related to these resources, please Ask a new question, and the NXP support team can address it there.

When learning Zephyr, there are lots of questions about memory.  Where does the linker place code and data?  How does the application configure to use other memories?

The default memory sections used by the linker are configured in the devicetree.  Typically the devicetree uses chosen nodes to configure these sections.  Here is an example from the board MIMXRT1060-EVK:

	chosen {
                zephyr,flash = &is25wp064;
                zephyr,sram = &sdram0;
	};

 

The names of these chosen nodes can be misleading.  zephyr,flash points to the node the linker uses for all the code (.text) and read-only data sections.  Typically this points to physical flash memory, like on this board it places in external QSPI flash, but it can be in memory that is not flash.  zephyr,sram points to the node the linker uses for all the .data and .bss sections.  This should be in RAM, but is not required to be in SRAM.  This board places in the external SDRAM.  The application can point these nodes to other memories that are best for that app.  Other common memory nodes used are &dtcm, &itcm, or &ocram. 

Typically, these chosen nodes are set in the board devicetree file.  But when learning Zephyr and working with devicetree, it is best to confirm the devicetree settings in the generated devicetree files created during the build of the application, see Lab Guide: Devicetree and VS Code Devicetree Viewer.

 

i.MX RT memory

Most memory questions come from those using the i.MX RT devices.  These MCUs are high-performance flashless devices with multiple internal and external memory options to maximize performance and flexibility for the application.  Some helpful resources specific to the i.MX RT devices:

  • i.MX RT application notes:
    • AN12437 i.MX RT Series Performance Optimization
    • AN12077 Using the i.MX RT FlexRAM
    • AN13970 RT Series Memory Relocation in Zephyr
  • The bootloader in ROM requires the Flash Configuration Block (FCB) when booting.  And optionally the Device Configuration Data (DCD) or eXternal Memory Configuration Data (XMCD) can be added, typically used to enable SDRAM.  This post has more details about where to find these structures, and how they are included with the board.
  • No SDRAM: the Zephyr support for RT development boards with external SDRAM typically place data in the SDRAM.  And the ROM bootloader will configure the SDRAM interface before the Zephyr app executes using the DCD or XMCD.  This post discusses removing the SDRAM for a custom board.
  • Configuring FlexRAM, resizing ITCM, DTCM, or OCRAM, see AN13970 RT Series Memory Relocation in Zephyr

 

Relocating code to RAM

Relocating code to RAM is a common requirement, like to maximize performance, or reduce power consumption.  With Zephyr, applications can relocate all the code, or part of the code to RAM.  Some helpful resources for relocation:

  • AN13970 RT Series Memory Relocation in Zephyr
  • Zephyr Code And Data Relocation APIs
  • Example applications that relocate code:
    • Simple example SDRAM_hello_world.zip that moves the entire app to SDRAM, and uses the ROM bootloader to load the RAM at boot, before the app executes.
    • Zperf sample: this networking sample in Zephyr relocates the networking stack and Ethernet driver code to ITCM to improve performance when built for the MIMXRT1170-EVK.  The rest of code remains in the default external QSPI flash.
    • NXP SmartWatch demo and webinar: relocates most code to internal SRAM to reduce power consumption, but leaves graphical assets in flash.

Locating data to RAM

With Zephyr, the default placement of all data, variables, and stacks go in the zephyr,sram node.  But some applications want some specific data to be placed elsewhere.  Like placing data in DTCM to maximize performance, placing a DMA buffer in non-cacheable memory, or moving large frame buffers for a display to external RAM.  Some helpful resources for specifying data placement include:

  • The declaration of static variables can include linker section tags to place them in specific sections.  A reference showing this is the dma_mcux_edma.c driver, which place the dma_tcdpool structures in the __dtcm_noinit_section or __nocache sections.
  • Another option for static variables is to use devicetree nodes in the variable declaration to place in a specific section.  One example to reference is NXP's Facial Detection demo.  This demo adds the chosen node zephyr,modelbuf in the devicetree, which points to the memory section node sramx.  To use this method, the memory section node requires the property zephyr,memory-region.  In the source code, the model_input_buf buffer is declared with the zephyr_modelbuf node.  Then the linker places model_input_buf in the sramx section.
  • The data and bss sections of entire source files or libraries can be relocated to other RAMs, see Zephyr Code And Data Relocation APIs.
  • Zephyr can use a special pinned section to place the interrupt and main stacks in a different RAM section.  The simple example pinned_hello_world.zip pins the interrupt and main stacks in DTCM.

 

Other memory resources

  • Example resizing memory nodes, leverages all SRAM in NXP LPC5500

 

Return to Zephyr Knowledge Hub

%3CLINGO-SUB%20id%3D%22lingo-sub-2008573%22%20slang%3D%22en-US%22%20mode%3D%22UPDATE%22%3EMemory%20details%20with%20Zephyr%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2008573%22%20slang%3D%22en-US%22%20mode%3D%22UPDATE%22%3E%0A%3CP%3E%3CSPAN%3EIf%20you%20have%20any%20questions%20or%20issues%20related%20to%20these%20resources%2C%20please%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project%2Fbd-p%2FZephyr-Project%22%20target%3D%22_blank%22%3EAsk%20a%20new%20question%3C%2FA%3E%3CSPAN%3E%2C%20and%20the%20NXP%20support%20team%20can%20address%20it%20there.%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EWhen%20learning%20Zephyr%2C%20there%20are%20lots%20of%20questions%20about%20memory.%26nbsp%3B%20Where%20does%20the%20linker%20place%20code%20and%20data%3F%26nbsp%3B%20How%20does%20the%20application%20configure%20to%20use%20other%20memories%3F%3C%2FP%3E%0A%3CP%3EThe%20default%20memory%20sections%20used%20by%20the%20linker%20are%20configured%20in%20the%20devicetree.%26nbsp%3B%20Typically%20the%20devicetree%20uses%20chosen%20nodes%20to%20configure%20these%20sections.%26nbsp%3B%20Here%20is%20an%20example%20from%20the%20board%20MIMXRT1060-EVK%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-css%22%3E%3CCODE%3E%09chosen%20%7B%0A%20%20%20%20%20%20%20%20%20%20%20%20%20%20%20%20zephyr%2Cflash%20%3D%20%26amp%3Bis25wp064%3B%0A%20%20%20%20%20%20%20%20%20%20%20%20%20%20%20%20zephyr%2Csram%20%3D%20%26amp%3Bsdram0%3B%0A%09%7D%3B%0A%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3EThe%20names%20of%20these%20chosen%20nodes%20can%20be%20misleading.%26nbsp%3B%20%3CCODE%3Ezephyr%2Cflash%3C%2FCODE%3E%20points%20to%20the%20node%20the%20linker%20uses%20for%20all%20the%20code%20(.text)%20and%20read-only%20data%20sections.%26nbsp%3B%20Typically%20this%20points%20to%20physical%20flash%20memory%2C%20like%20on%20this%20board%20it%20places%20in%20external%20QSPI%20flash%2C%20but%20it%20can%20be%20in%20memory%20that%20is%20not%20flash.%26nbsp%3B%20%3CCODE%3Ezephyr%2Csram%3C%2FCODE%3E%20points%20to%20the%20node%20the%20linker%20uses%20for%20all%20the%20.data%20and%20.bss%20sections.%26nbsp%3B%20This%20should%20be%20in%20RAM%2C%20but%20is%20not%20required%20to%20be%20in%20SRAM.%26nbsp%3B%20This%20board%20places%20in%20the%20external%20SDRAM.%26nbsp%3B%20The%20application%20can%20point%20these%20nodes%20to%20other%20memories%20that%20are%20best%20for%20that%20app.%26nbsp%3B%20Other%20common%20memory%20nodes%20used%20are%20%3CCODE%3E%26amp%3Bdtcm%3C%2FCODE%3E%2C%20%3CCODE%3E%26amp%3Bitcm%3C%2FCODE%3E%2C%20or%20%3CCODE%3E%26amp%3Bocram%3C%2FCODE%3E.%26nbsp%3B%3C%2FP%3E%0A%3CP%3ETypically%2C%20these%20chosen%20nodes%20are%20set%20in%20the%20board%20devicetree%20file.%26nbsp%3B%20But%20when%20learning%20Zephyr%20and%20working%20with%20devicetree%2C%20it%20is%20best%20to%20confirm%20the%20devicetree%20settings%20in%20the%20generated%20devicetree%20files%20created%20during%20the%20build%20of%20the%20application%2C%20see%20%3CA%20href%3D%22https%3A%2F%2Fmcuxpresso.nxp.com%2Fmcux-vscode%2Flatest%2Fhtml%2FTraining-Zephyr-Getting-Started.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ELab%20Guide%3A%20Devicetree%20and%20VS%20Code%20Devicetree%20Viewer%3C%2FA%3E.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CH2%20id%3D%22toc-hId--557348501%22%20id%3D%22toc-hId--499197399%22%3Ei.MX%20RT%20memory%3C%2FH2%3E%0A%3CP%3EMost%20memory%20questions%20come%20from%20those%20using%20the%20i.MX%20RT%20devices.%26nbsp%3B%20These%20MCUs%20are%20high-performance%20flashless%20devices%20with%20multiple%20internal%20and%20external%20memory%20options%20to%20maximize%20performance%20and%20flexibility%20for%20the%20application.%26nbsp%3B%20Some%20helpful%20resources%20specific%20to%20the%20i.MX%20RT%20devices%3A%3C%2FP%3E%0A%3CUL%3E%0A%3CLI%3Ei.MX%20RT%20application%20notes%3A%0A%3CUL%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN12437.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN12437%3C%2FA%3E%26nbsp%3Bi.MX%20RT%20Series%20Performance%20Optimization%3C%2FLI%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN12077.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN12077%3C%2FA%3E%20Using%20the%20i.MX%20RT%20FlexRAM%3C%2FLI%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fdocs.nxp.com%2Fbundle%2FAN14597%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EAN13970%3C%2FA%3E%26nbsp%3BRT%20Series%20Memory%20Relocation%20in%20Zephyr%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3C%2FLI%3E%0A%3CLI%3EThe%20bootloader%20in%20ROM%20requires%20the%20Flash%20Configuration%20Block%20(FCB)%20when%20booting.%26nbsp%3B%20And%20optionally%20the%26nbsp%3BDevice%20Configuration%20Data%20(DCD)%20or%20eXternal%20Memory%20Configuration%20Data%20(XMCD)%20can%20be%20added%2C%20typically%20used%20to%20enable%20SDRAM.%26nbsp%3B%20This%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F83607%23discussioncomment-11754808%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Epost%3C%2FA%3E%20has%20more%20details%20about%20where%20to%20find%20these%20structures%2C%20and%20how%20they%20are%20included%20with%20the%20board.%3C%2FLI%3E%0A%3CLI%3ENo%20SDRAM%3A%20the%20Zephyr%20support%20for%20RT%20development%20boards%20with%20external%20SDRAM%20typically%20place%20data%20in%20the%20SDRAM.%26nbsp%3B%20And%20the%20ROM%20bootloader%20will%20configure%20the%20SDRAM%20interface%20before%20the%20Zephyr%20app%20executes%20using%20the%20DCD%20or%20XMCD.%26nbsp%3B%20This%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F61816%23discussioncomment-6852726%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Epost%3C%2FA%3E%20discusses%20removing%20the%20SDRAM%20for%20a%20custom%20board.%3C%2FLI%3E%0A%3CLI%3EConfiguring%20FlexRAM%2C%20resizing%20ITCM%2C%20DTCM%2C%20or%20OCRAM%2C%20see%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fdocs.nxp.com%2Fbundle%2FAN14597%2Fpage%2Ftopics%2Fintroduction.html%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EAN13970%3C%2FA%3E%26nbsp%3BRT%20Series%20Memory%20Relocation%20in%20Zephyr%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CBR%20%2F%3E%0A%3CH2%20id%3D%22toc-hId-1930164332%22%20id%3D%22toc-hId-1988315434%22%3ERelocating%20code%20to%20RAM%3C%2FH2%3E%0A%3CP%3ERelocating%20code%20to%20RAM%20is%20a%20common%20requirement%2C%20like%20to%20maximize%20performance%2C%20or%20reduce%20power%20consumption.%26nbsp%3B%20With%20Zephyr%2C%20applications%20can%20relocate%20all%20the%20code%2C%20or%20part%20of%20the%20code%20to%20RAM.%26nbsp%3B%20Some%20helpful%20resources%20for%20relocation%3A%3C%2FP%3E%0A%3CUL%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fdocs.nxp.com%2Fbundle%2FAN14597%2Fpage%2Ftopics%2Fintroduction.html%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EAN13970%3C%2FA%3E%26nbsp%3BRT%20Series%20Memory%20Relocation%20in%20Zephyr%3C%2FLI%3E%0A%3CLI%3EZephyr%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fkernel%2Fcode-relocation.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ECode%20And%20Data%20Relocation%20APIs%3C%2FA%3E%3C%2FLI%3E%0A%3CLI%3EExample%20applications%20that%20relocate%20code%3A%0A%3CUL%3E%0A%3CLI%3ESimple%20example%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F78948%23discussioncomment-10823905%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ESDRAM_hello_world.zip%3C%2FA%3E%26nbsp%3Bthat%20moves%20the%20entire%20app%20to%20SDRAM%2C%20and%20uses%20the%20ROM%20bootloader%20to%20load%20the%20RAM%20at%20boot%2C%20before%20the%20app%20executes.%3C%2FLI%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fsamples%2Fnet%2Fzperf%2FREADME.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EZperf%20sample%3C%2FA%3E%3A%20this%20networking%20sample%20in%20Zephyr%20relocates%20the%20networking%20stack%20and%20Ethernet%20driver%20code%20to%20ITCM%20to%20improve%20performance%20when%20built%20for%20the%20MIMXRT1170-EVK.%26nbsp%3B%20The%20rest%20of%20code%20remains%20in%20the%20default%20external%20QSPI%20flash.%3C%2FLI%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Ftraining%2Fdesigning-for-low-power-using-zephyr-project-a-smartwatch-example%3ATIP-DESIGN-LOW-POWER-ZEPHYR-SMARTWATCH%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ENXP%20SmartWatch%20demo%20and%20webinar%3C%2FA%3E%3A%20relocates%20most%20code%20to%20internal%20SRAM%20to%20reduce%20power%20consumption%2C%20but%20leaves%20graphical%20assets%20in%20flash.%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId-122709869%22%20id%3D%22toc-hId-180860971%22%3ELocating%20data%20to%20RAM%3C%2FH2%3E%0A%3CP%3EWith%20Zephyr%2C%20the%20default%20placement%20of%20all%20data%2C%20variables%2C%20and%20stacks%20go%20in%20the%20%3CCODE%3Ezephyr%2Csram%3C%2FCODE%3E%20node.%26nbsp%3B%20But%20some%20applications%20want%20some%20specific%20data%20to%20be%20placed%20elsewhere.%26nbsp%3B%20Like%20placing%20data%20in%20DTCM%20to%20maximize%20performance%2C%20placing%20a%20DMA%20buffer%20in%20non-cacheable%20memory%2C%20or%20moving%20large%20frame%20buffers%20for%20a%20display%20to%20external%20RAM.%26nbsp%3B%20Some%20helpful%20resources%20for%20specifying%20data%20placement%20include%3A%3C%2FP%3E%0A%3CUL%3E%0A%3CLI%3EThe%20declaration%20of%20static%20variables%20can%20include%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fblob%2Fmain%2Finclude%2Fzephyr%2Flinker%2Fsection_tags.h%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Elinker%20section%20tags%3C%2FA%3E%20to%20place%20them%20in%20specific%20sections.%26nbsp%3B%20A%20reference%20showing%20this%20is%20the%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fblob%2Fmain%2Fdrivers%2Fdma%2Fdma_mcux_edma.c%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Edma_mcux_edma.c%3C%2FA%3E%20driver%2C%20which%20place%20the%20%3CCODE%3Edma_tcdpool%3C%2FCODE%3E%20structures%20in%20the%20%3CCODE%3E__dtcm_noinit_section%3C%2FCODE%3E%20or%20%3CCODE%3E__nocache%3C%2FCODE%3E%20sections.%3C%2FLI%3E%0A%3CLI%3EAnother%20option%20for%20static%20variables%20is%20to%20use%20devicetree%20nodes%20in%20the%20variable%20declaration%20to%20place%20in%20a%20specific%20section.%26nbsp%3B%20One%20example%20to%20reference%20is%20NXP's%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fnxp-zephyr%2Fapps_zephyr%2Ftree%2FFacialDetect%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EFacial%20Detection%20demo%3C%2FA%3E.%26nbsp%3B%20This%20demo%20adds%20the%20chosen%20node%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fnxp-zephyr%2Fapps_zephyr%2Fblob%2FFacialDetect%2Fapps%2FFacialDetect%2Fboards%2Ffrdm_mcxn947_mcxn947_cpu0.overlay%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3E%3CCODE%3Ezephyr%2Cmodelbuf%3C%2FCODE%3E%3C%2FA%3E%20in%20the%20devicetree%2C%20which%20points%20to%20the%20memory%20section%20node%20%3CCODE%3Esramx%3C%2FCODE%3E.%26nbsp%3B%20To%20use%20this%20method%2C%20the%20memory%20section%20node%20requires%20the%20property%20%3CCODE%3Ezephyr%2Cmemory-region%3C%2FCODE%3E.%26nbsp%3B%20In%20the%20source%20code%2C%20the%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fnxp-zephyr%2Fapps_zephyr%2Fblob%2F1bd145a0792134b34612f16b7b8a25c76c52aac2%2Fapps%2FFacialDetect%2Fsrc%2Fface_det.cpp%23L107C16-L107C31%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3E%3CCODE%3Emodel_input_buf%3C%2FCODE%3E%3C%2FA%3E%20buffer%20is%20declared%20with%20the%20%3CCODE%3Ezephyr_modelbuf%3C%2FCODE%3E%20node.%26nbsp%3B%20Then%20the%20linker%20places%20%3CCODE%3Emodel_input_buf%3C%2FCODE%3E%20in%20the%20%3CCODE%3Esramx%3C%2FCODE%3E%20section.%3C%2FLI%3E%0A%3CLI%3EThe%20data%20and%20bss%20sections%20of%20entire%20source%20files%20or%20libraries%20can%20be%20relocated%20to%20other%20RAMs%2C%20see%26nbsp%3BZephyr%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fkernel%2Fcode-relocation.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ECode%20And%20Data%20Relocation%20APIs%3C%2FA%3E.%3C%2FLI%3E%0A%3CLI%3EZephyr%20can%20use%20a%20special%20pinned%20section%20to%20place%20the%20interrupt%20and%20main%20stacks%20in%20a%20different%20RAM%20section.%26nbsp%3B%20The%20simple%20example%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F81162%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Epinned_hello_world.zip%3C%2FA%3E%26nbsp%3Bpins%20the%20interrupt%20and%20main%20stacks%20in%20DTCM.%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId--1684744594%22%20id%3D%22toc-hId--1626593492%22%3E%26nbsp%3B%3C%2FH2%3E%0A%3CH2%20id%3D%22toc-hId-802768239%22%20id%3D%22toc-hId-860919341%22%3EOther%20memory%20resources%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F73539%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EExample%3C%2FA%3E%20resizing%20memory%20nodes%2C%20leverages%20all%20SRAM%20in%20NXP%20LPC5500%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CBR%20%2F%3E%0A%3CP%3EReturn%20to%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project-Knowledge-Base%2FZephyr-Support-Resources%2Fta-p%2F2008548%22%20target%3D%22_blank%22%3EZephyr%20Knowledge%20Hub%3C%2FA%3E%3C%2FP%3E%0A%3C%2FLINGO-BODY%3E
100% helpful (1/1)
Version history
Last update:
‎12-19-2025 08:39 AM
Updated by: