xiaomi door sensor leave instead rejoin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

xiaomi door sensor leave instead rejoin

7,674件の閲覧回数
admin-23
Contributor I

Hello friends! I have a similar situation, like in https://community.nxp.com/t5/Wireless-Connectivity/zigbee-rejoin/m-p/1151456#M10135

I have 10 psc xiaomi door/window sensor, connected to gate, based on lumi (jn5169 chip). Software is Zigate firmware - https://github.com/fairecasoimeme/ZiGate

Problem was described in detail - https://github.com/fairecasoimeme/ZiGate/issues/349

Briefly, as a result, if the device did not show signs of life for 1-4 hours, then the coordinator will kick it out of the network and ask to restart it, but not all devices come back. In the exchange protocol, we see only a message about the exit from the network, but not about the fact that the exit was initiated by the coordinator himself.

Other xiaomi sensors (temp/humidity, occupancy sensor, etc) in my situation, based on jn5169 works well.

Can i modify Zigate Coordinator source code (based on JN-AN-1216) so that xiaomi door sensors NOT leave Coordinator (will rejoin instead leave)

0 件の賞賛
返信
3 返答(返信)

7,649件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @admin-23,

It seems a similar issue that the community thread that you shared previously.

The coordinator receives a timeout from each device, so the next time that the device wakes up,  the coordinator will send a leave command.

Do you capture the packets over the air?

Can i modify Zigate Coordinator source code (based on JN-AN-1216) so that xiaomi door sensors NOT leave Coordinator (will rejoin instead leave)

It is part of the Zigbee specification.

Regards,

Mario

0 件の賞賛
返信

7,608件の閲覧回数
admin-23
Contributor I

After 3 hours coordinator power off, door sensor 0xd636 leave ..

0 件の賞賛
返信

7,593件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @admin-23,

Is it possible that you could provide the sniffer file?

What is the timeout value that you have when the door sensor joins the network?

Regards,

Mario

0 件の賞賛
返信