wireless transmitter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wireless transmitter

3,225 Views
thomasweger
Contributor I

Dear Sir or Madame, I would like to use a wireless transmitter (e.g. NXQ1TXH5 ) and the corresponding receiver  in an application where the receiver is spinning around his axe with approximately 9000 rounds per minute. Is this possible with your device or has the receiver and transmitter be static (although air gab is not changing)? Thank you very much four your support.

1 Reply

3,090 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

There should not be any problem from the wireless transmitter (e.g. NXQ1TXH5DB1401), the question would be if there could be a problem with the wireless receiver while trying to receive the data while spinning.

 

I checked with our applications engineers and they confirmed that we have never tested shuck application, but, they believe that there should not be any problem with it since the both transmitter and receiver are omni-directional. Since we have never tested before, I’m afraid that you would need to perform your own tests.

Regards,
Jose