whether the AN1210_CustomerModuleEvalTool could add 2dBm-3dBm based on Power Level 3 setting?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

whether the AN1210_CustomerModuleEvalTool could add 2dBm-3dBm based on Power Level 3 setting?

1,571件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Customer want to set their board output power is about 20dBm, but they could not achieve it by AN1210_CustomerModuleEvalTool.

When set power Level  4------Test their board RF output is about 22.4dBm.

When set power Level  3------ Test their board RF output is about 12.7dBm. At this situation, we could set the 2.5dBm attenuator off,  Default Tx Power +1.6dBm, but the output is just 16.8dBm (12.7+2.5+1.6). 

Could you help check whether the CMET tools could add 2dBm-3dBm based on Power Level value 3 ?

ラベル(2)
0 件の賞賛
返信
1 返信

1,364件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Hanson,

Which board are you using? Are you referring the AN1210 app note?

Regards,

Mario

0 件の賞賛
返信