whether the AN1210_CustomerModuleEvalTool could add 2dBm-3dBm based on Power Level 3 setting?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

whether the AN1210_CustomerModuleEvalTool could add 2dBm-3dBm based on Power Level 3 setting?

1,574 Views
hansonhe
NXP Employee
NXP Employee

Customer want to set their board output power is about 20dBm, but they could not achieve it by AN1210_CustomerModuleEvalTool.

When set power Level  4------Test their board RF output is about 22.4dBm.

When set power Level  3------ Test their board RF output is about 12.7dBm. At this situation, we could set the 2.5dBm attenuator off,  Default Tx Power +1.6dBm, but the output is just 16.8dBm (12.7+2.5+1.6). 

Could you help check whether the CMET tools could add 2dBm-3dBm based on Power Level value 3 ?

0 Kudos
Reply
1 Reply

1,367 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Hanson,

Which board are you using? Are you referring the AN1210 app note?

Regards,

Mario

0 Kudos
Reply