using clock() function time.h in BeyondStudio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using clock() function time.h in BeyondStudio

2,243件の閲覧回数
LUIPS
Contributor I

I am trying to use time.h file clock() function. to get the running time of the program。However,when i build the project,it shows the following errors:

/ba_toolchain/r36379/source/gcc-4.7.4-ba-r36379-build/ba-elf/mcpu_jn51xx_sizeopt/newlib/libc/sys/basim/../../../../../../../gcc-4.7.4-ba-r36379/newlib/libc/sys/basim/glue.c:75: undefined reference to `end'
/ba_toolchain/r36379/source/gcc-4.7.4-ba-r36379-build/ba-elf/mcpu_jn51xx_sizeopt/newlib/libc/sys/basim/../../../../../../../gcc-4.7.4-ba-r36379/newlib/libc/sys/basim/glue.c:75: undefined reference to `_stack'
/ba_toolchain/r36379/source/gcc-4.7.4-ba-r36379-build/ba-elf/mcpu_jn51xx_sizeopt/newlib/libc/sys/basim/../../../../../../../gcc-4.7.4-ba-r36379/newlib/libc/sys/basim/glue.c:75: undefined reference to `_stack'
/ba_toolchain/r36379/source/gcc-4.7.4-ba-r36379-build/ba-elf/mcpu_jn51xx_sizeopt/newlib/libc/sys/basim/../../../../../../../gcc-4.7.4-ba-r36379/newlib/libc/sys/basim/glue.c:75:(.text+0x197): relocation truncated to fit: R_BA_8 against undefined symbol `_stack'

Could anyone tell me how to solve this problem ?

タグ(1)
0 件の賞賛
返信
1 返信

2,223件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please take a look at the following document for information about BeyondStudio Common Errors?

 

What Application Note are you using as a base? What modifications did you do?

 

Also, we highly recommend moving to the JN5189 Wireless MCU for Zigbee® and Thread, as is our focus part for ZigBee/Thread. It is supported by our MCUXpresso IDE and MCUXpresso SDK. There are several SDK examples, like driver examples (GPIO, UART, SPI, I2C), RTOS examples, and Wireless examples (ZigBee and Thread).

 

Regards,

Ricardo

0 件の賞賛
返信