undefined reference to `eHA_RegisterIASWarningDeviceEndPoint'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

undefined reference to `eHA_RegisterIASWarningDeviceEndPoint'

6,074 Views
chen217800
Contributor I

Building can't Success.It show like this:

Building trace version ...
Linking /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Router_JN5169_DRZG15.elf ...
/c/NXP/bstudio_nxp/sdk/Tools/ba-elf-ba2-r36379/bin/ba-elf-gcc -Wl,--gc-sections -Wl,-u_AppColdStart -Wl,-u_AppWarmStart -march=ba2 -mcpu=jn51xx -mredzone-size=4 -mbranch-cost=3 -fomit-frame-pointer -Os -fshort-enums -flto  -nostartfiles -L/c/NXP/bstudio_nxp/sdk/JN-SW-4170/Chip/JN5169/Build -L/c/NXP/bstudio_nxp/sdk/JN-SW-4170/Chip/JN5169/Library -L/c/NXP/bstudio_nxp/sdk/JN-SW-4170/Components/Library -Wl,--gc-sections -L/c/NXP/bstudio_nxp/sdk/JN-SW-4170/Stack/ZBPro/Build -Wl,--defsym=__stack_size=5000 -Wl,--defsym,__minimum_heap_size=2000 -L /c/NXP/bstudio_nxp/sdk/JN-SW-4170/Stack/ZCL/Build/ -TAppBuildZBPro.ld -o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Router_JN5169_DRZG15.elf -Wl,--start-group /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/app_main.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/irq_JN516x.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/portasm_JN516x.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/port_JN516x.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/pdum_gen.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/pdum_apdu.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zps_gen.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/app_start.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/app_router_node.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/app_zcl_task.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/app_buttons.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/app_led_interface.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/IASWDBoard.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/ZQueue.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/ZTimer.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/app_zps_link_keys.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Alarms.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/AlarmsClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/AlarmsCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/AlarmsServerCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/AlarmsTableManager.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/AnalogInputBasic.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/AnalogOutputBasic.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Basic.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/BasicClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/BasicCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/BinaryInputBasic.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/BinaryOutputBasic.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/DeviceTemperatureConfiguration.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Diagnostics.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Groups.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/GroupsClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/GroupsCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/GroupsServerCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/GroupsTableManager.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Identify.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/IdentifyClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/IdentifyCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/IdentifyServerCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/LevelControl.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/LevelControlClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/LevelControlCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/MultistateInputBasic.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/MultistateOutputBasic.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/OOSC.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/OnOff.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/OnOffCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/OnOffCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PollControl.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PollControlClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PollControlCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PollControlServerCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PowerConfiguration.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PowerProfile.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PowerProfileClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PowerProfileCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/PowerProfileServerCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Scenes.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/ScenesClientCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/ScenesClusterManagement.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/ScenesCommandHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/ScenesServerCommands.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/ScenesTableManager.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/TC.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Time.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/base_device.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/mains_power_outlet.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/on_off_output.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/plug_control.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/remote_control.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/simple_sensor.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/dlist.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_CustomCommandReceive.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_CustomCommandSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_PDUbufferReadWrite.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_PDUbufferReadWriteString.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_WriteAttributesRequestHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_WriteAttributesRequestSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_WriteAttributesResponseHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_attribute.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_buffer.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_clusterCommand.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_command.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_common.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_configureReportingCommandHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_configureReportingCommandSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_configureReportingResponseHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_defaultResponse.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverAttributesExtendedRequestHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverAttributesExtendedRequestSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverAttributesExtendedResponseHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverAttributesRequestHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverAttributesRequestSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverAttributesResponseHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverCommandsRequestHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverCommandsRequestSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_discoverCommandsResponseHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_event.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_heap.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_library_options.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_readAttributesRequestHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_readAttributesRequestSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_readAttributesResponseHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_readReportingConfigurationCommandHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_readReportingConfigurationCommandSend.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_readReportingConfigurationResponseHandle.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_reportManager.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_reportMaths.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_reportScheduler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_reportStringHandling.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_reportStructure.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_search.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_timer.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/zcl_transmit.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/bdb_fr.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/bdb_start.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/bdb_state_machine.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/appZpsBeaconHandler.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/appZdpExtraction.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/bdb_ns.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/bdb_nf.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/bdb_fb_common.o /c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/bdb_fb_target.o -lZPSMAC_Mini_SOC_JN516x -lPWRM_JN516x -lZPSTSV_JN516x -lAES_SW_JN516x -lPDUM_JN516x -lZPSAPL_JN516x -lRandom_JN516x -lPDM_EEPROM_NO_RTOS_JN516x -lDBG_JN516x -lZPSNWK_JN516x -lMiniMac_JN5169 -lMiniMacShim_JN516x -lMMAC_JN5169 -lJPT_JN5169 -lAes_JN516x -lHardwareApi_JN5169 -lMicroSpecific_JN516x -lBoot_JN516x -lJPT_JN5169 -lm -Wl,--end-group -Wl,-Map,Router_JN5169_DRZG15.map
C:\Users\chenyk\AppData\Local\Temp\ccr0foth.ltrans0.ltrans.o: In function `AppColdStart':
ccr0foth.ltrans0.o:(.text+0x17fa): undefined reference to `eHA_RegisterIASWarningDeviceEndPoint'
ccr0foth.ltrans0.o:(.text+0x17fa): relocation truncated to fit: R_BA_18_PCREL against undefined symbol `eHA_RegisterIASWarningDeviceEndPoint'
collect2.exe: error: ld returned 1 exit status
make: *** [/c/NXP/bstudio_nxp/workspace/JN-AN-1217-Zigbee-3-0-Base-Device/Router/Build/Router_JN5169_DRZG15.elf] Error 1
17:54:11 Build Finished (took 35s.729ms)
---------------------------------------------------------------------
  • Attached is my configuration! my SDK is JN-SW-4141 BeyondStudio for NXP v1308 and JN-SW-4170 Zigbee 3.0 v1840

Tags (1)
0 Kudos
Reply
1 Reply

5,911 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Chenyk,

Did you add the warning_device.h/.c files?

C:\NXP\bstudio_nxp\sdk\JN-SW-4168\Components\ZCL\Profiles\HA\IAS

Regards,

Mario

0 Kudos
Reply