problem when import JN-AN-1217

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem when import JN-AN-1217

1,495 Views
LeoMe
Contributor I

im working on jn5169 development using beyondstudio

when i try to import JN-AN-1217,and select jn516x platform,the beyondstudio project explorer display something not right,like this

QQ截图20211028114841.png

you can see there are no source file imported

but when i select jn517x platform,it works good

QQ截图20211028114738.png

and this is my import window

QQ截图20211028114825.png

0 Kudos
Reply
1 Reply

1,487 Views
nxf56274
NXP Employee
NXP Employee

Hi,

工程里就这么多文件,其他的一些运行函数都放在bstudio_nxp\sdk下,这个链接包含了大部分内容,https://www.nxp.com/pages/jn516x-7x-zigbee-3-0:ZIGBEE-3-0

0 Kudos
Reply