op EraseSector error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

op EraseSector error

1,642件の閲覧回数
toru148
Contributor I

I got error message :

EraseSector (0x0, 0x0, 0x1) status 0x40 - driver reports init failure - ONCHIP driver rc 104 (0x68)

complains because another operation was called after Init failed (status 0x40)

Do you know how to fix?

I tried mass-erase on GUI Flash Tool, but it does not fix this issue.

Sample : qn908xcdk_wireless_examples_bluetooth_beacon_freertos

IDE : MCUXpresso IDE v11.0.1 [Build 2563] [2019-09-01]

Board : QN9080SIP Development kit

OS : MacOS 10.14.6

ラベル(2)
0 件の賞賛
返信
1 返信

1,561件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Toru, I hope you're doing well!

 

Could you please try programming the device with the ISP pins (JP15) shorted during a reset?

 

Also, which debug probe are you using?

 

What firmware did you last program?

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 件の賞賛
返信