kw32w041 not booting when GPIO5 is held low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kw32w041 not booting when GPIO5 is held low

1,670件の閲覧回数
jacinto1m
Contributor II

Hi,

I am wondering whether there is anything the the NXP bootloader that prevents the kw32w041 to boot up when I put low the GPIO5 before powering it up.

Any help is much appreciated.

ラベル(1)
  • JN

0 件の賞賛
返信
1 返信

1,658件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. The GPIO5 is also the ISP Entry pin:

Ricardo_Zamora_1-1623861987378.png

[3] ISP programming mode: leave pin floating high during reset to avoid entering UART programming mode or hold it low to program

 

You can find this information in the Data Sheet.

 

Best Regards,

Ricardo

0 件の賞賛
返信