jn5169 zigbee3.0 Transfer Size

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

jn5169 zigbee3.0 Transfer Size

2,657 次查看
1516998341
Contributor I

I am currently working on the development of zigbee 3.0 at beyond Studio jn5169. I have a question about zigbee's maximum transmission data.My questions are as follows:

1. Can the maximum transmission size be modified?

2. If the Transfer Size can be changed, should I modify Maximun Transfer Size in the configuration parameters of Node Descriptor in app.zpscfg file?As is shown in

pastedImage_1.png

3. If it is like what I said, but I cannot change the Maximun incoming Transfer Size parameter, please inform me how to modify it

0 项奖励
回复
3 回复数

2,565 次查看
1516998341
Contributor I

I wonder if you have misunderstood my meaning. I wonder if it is possible to modify the two parameters of "Maximum Incoming Transfer Size" and "Maximum Outgoing Transfer Size" in the picture?Or how to modify these two parameters?

pastedImage_1.png

0 项奖励
回复

2,565 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Adding comments form patrickpan‌

Maximum incoming transfer size. The maximum incoming transfer size supported by the device. This is calculated from the APDU sizes for input clusters. Not editable.

Look at the PDU Manager

pastedImage_1.png

ZigBee PRO Stack User Guide For better details look at the Chapter 10.7.6 Node Descriptor

Regards,

Mario

0 项奖励
回复

2,565 次查看
patrick_pan
NXP Employee
NXP Employee

From your app.zpscfg , it is based on AN1218 which is mainly for ZR node ,but you added one ZED configuration .

Strongly suggest not do like that way , if you want to deploy ZED you can pick app.zpscfg either from AN1219 or AN1220, depending what kind of node you want to develop.

0 项奖励
回复