getting Instruction error when build JN5168 zigbee endpoint application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

getting Instruction error when build JN5168 zigbee endpoint application

3,557件の閲覧回数
ravikumarv
Contributor I

Dear Sir,

I am facing a typical problem while working on JN5168 module.

I a using NXP base device examples for testing ZIGBEE, i have build applications one as coordinator and other as Endpoint.
First i have loaded the coordinator.bin file into JN5168 module and able to see the network formation success using channel 11.

Next i have done factory reset to the board and loaded Endpoint application, but system is crashing at ZPS_eAplAfInit() call.

I am able to see the below message

***********************************************
* END DEVICE RESET *
***********************************************
APP: Entering APP_vInitResources()
APP: Entering APP_vSetUpHardware()
APP: Entering APP_vInitialise()
APP: Entering APP_ZCL_vInitialise()
APP: Entering ZPS_eAplAfInit()

!!! Instruction error
u32PICMR = 0 : u32PICSR = 8008
u32PICMSR = 0 : u32IPMR = 0
u32IHPR = c : u32AINT = 8008 u32PINT 0
EPCR = 0 : EEAR = 0
Stack dump:
4007d18 : 040012c8
4007d1c : 00000000
4007d20 : 00000000
4007d24 : 00000000
4007d28 : 0000000c
4007d2c : 00000000
4007d30 : 00008008
4007d34 : 00000000
4007d38 : 00000000
4007d3c : 00008008
4007d40 : 00000003
4007d44 : 0009b233
4007d48 : 04001fec
4007d4c : 00082519
4007d50 : 040005fc
4007d54 : ffffffff
4007d58 : ffffffff
4007d5c : ffffffff
4007d60 : ffffffff
4007d64 : ffff1504
4007d68 : 00000000
4007d6c : 00000002
4007d70 : 00000002
4007d74 : 00000000
4007d78 : 01ffffff
4007d7c : 010000c8
4007d80 : 01ffffff
4007d84 : 00000000
4007d88 : 00000000
4007d8c : 00000000
4007d90 : 00000000
4007d94 : 0000000d
4007d98 : 00000014
4007d9c : 00080218
4007da0 : 00000000
4007da4 : 00000000
4007da8 : 00000007
4007dac : 00000000
4007db0 : 00000000
4007db4 : 00000000
4007db8 : 00000000
4007dbc : ff00ffff
4007dc0 : f1060134
4007dc4 : 66000003

0 件の賞賛
返信
4 返答(返信)

3,189件の閲覧回数
cj_veeneman
Contributor II

Good Day Mario; I have this problem as well.

JN5169, JN-AN-1217(v1005), EndDevice

in APP_vInitialiseNode():

// debug msg here appears

ZPS_eAplAfInit();

// not reached, debug msg here will not appear.

attached is the Stack dump
Is there a utility that I can decode / trace the stack dump ?
Thank you in advance for any help you are able to provide.

0 件の賞賛
返信

3,189件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Christopher,

I hope you are doing great.

Is it possible that you could post this issue in a new community post?

Could you please explain the issue that you are facing and how you are getting this issue?

What is the SDK version that you are working on?

Regards,

Mario

0 件の賞賛
返信

3,189件の閲覧回数
cj_veeneman
Contributor II

sure, will do.

0 件の賞賛
返信

3,189件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ravi,


What is the application note that you took as a reference?

Best Regards,

Mario

0 件の賞賛
返信