eHA_RegisterSmartPlugEndPoint() ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eHA_RegisterSmartPlugEndPoint() ERROR

2,825件の閲覧回数
小鹏陈
Contributor II

Hello everybody,

   When i use the function eHA_RegisterSmartPlugEndPoint() to register device,   console display some message:

ccsbRm5s.ltrans0.o:(.text+0x1692): undefined reference to `au8SimpleMeteringServerAttributeControlBits'
ccsbRm5s.ltrans0.o:(.text+0x16a6): undefined reference to `sCLD_SimpleMetering'
ccsbRm5s.ltrans0.o:(.text+0x16ab): undefined reference to `sCLD_SimpleMetering'
ccsbRm5s.ltrans0.o:(.text+0x16af): undefined reference to `eSE_SMCreate'
ccsbRm5s.ltrans0.o:(.text+0x16af): relocation truncated to fit: R_BA_18_PCREL against undefined symbol eSE_SMCreate'

collect2.exe: error: ld returned 1 exit status

タグ(2)
3 返答(返信)

2,614件の閲覧回数
jonw1
Contributor II

Mario,

I am having this issue as well. I am getting the same exact build errors when adding the simple metering cluster to my project. I am developing with JN-AN-1217-Zigbee-3-0-Base-Device.

Best Regards,
Jonathan Witthoeft

0 件の賞賛
返信

2,614件の閲覧回数
jonw1
Contributor II

I found the problem was I did not have this line un-commented in the default project make file:
APP_CLUSTERS_SMART_ENERGY_SRC               ?= 1

As soon as I added it, it compiled.

2,614件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Chris,

Could you please share the implementation that you are doing? Also, what is the application that you are working on? are you working with the JN-AN-1216 Control bridge?

Regards,

Mario

0 件の賞賛
返信