cygwin heap error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cygwin heap error

1,896 Views
vishnubeema
Contributor III

Hello,

I was working on smac connectivity test application code. It was able to compile and working fine. But suddenly I started getting below error. Even if I compile other example codes, I am getting below error. Pleas let me know why this kind of issues will occur and how to fix. 

16:36:29 **** Build of configuration Debug for project frdmkw41z_wireless_examples_smac_connectivity_test_freertos ****

make -r -j4 all

m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x480000, m.State 0x10000

C:\nxp\MCUXpressoIDE_10.0.2_411\ide\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2E10000>) in child, Win32 error 0

m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x480000, m.State 0x10000

C:\nxp\MCUXpressoIDE_10.0.2_411\ide\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2BD0000>) in child, Win32 error 0

m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x480000, m.State 0x10000

C:\nxp\MCUXpressoIDE_10.0.2_411\ide\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2C00000>) in child, Win32 error 0

m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x480000, m.State 0x10000

C:\nxp\MCUXpressoIDE_10.0.2_411\ide\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2BD0000>) in child, Win32 error 0

make: *** [utilities/fsl_debug_console.o] Error 1

make: *** Waiting for unfinished jobs....

make: *** [startup/startup_MKW41Z4.o] Error 1

make: *** [source/connectivity_test.o] Error 1

make: *** [source/connectivity_test_menus.o] Error 1

 

16:36:31 Build Finished (took 1s.360ms)

 

Thanks & Regards

Vishnu Beema

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,649 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Could you please let me know which OS are you using? Also, which version of the SDK are you using?  

Best regards, 

Estephania 

0 Kudos
Reply