application note AN12657 "Using the RC663 without library"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

application note AN12657 "Using the RC663 without library"

2,028件の閲覧回数
madid
Contributor I

Hello, I implemented the example 4.2.1 example code - Inventory -ISO15693 of the application note AN12657 about the NFC reader MFRC630 without success. Please, can you clarify step 15 "The function CardResponded reads the IRQ0 register , which indicates if a card has responded or not"? What are the IRQ0 register bits to test? Second point: there is a scripting file for NFC Cockpit to achieve the same result of the example above?

0 件の賞賛
返信
2 返答(返信)

2,010件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi  @madid 

 Please refer to IRQ0 register details,

 

danielchen_1-1656666107891.png

For how to check CardResponse

danielchen_2-1656666181895.png

 

Regards

Daniel

 

 

 

 

0 件の賞賛
返信

1,993件の閲覧回数
madid
Contributor I

Hello,

I did not solve the problem. The interrupt does not trigger; I am very disappointed that an example of an official NXP application does not work

Best regards

0 件の賞賛
返信