about KW45 Freq Range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about KW45 Freq Range

2,018 Views
Annie_he
Contributor III

Hi NXP,

    We will use KW45 blurtooth board to get certification SRRC.

    But now when we test Frequency Range and Found that is is out of the lower limit, which is requested Less than -30dBm/100Khz, and its requested Frenquency is more than 2400Mhz, when operating in 2402Mhz. 

    And We test result as below:

1M(when power=-30.120, its freq error=2.400971GHz>2.4GHz, pass and The margin is sufficient)

Annie_he_0-1714034502913.png

2M(when power=-30.03, its freq error=2.400015GHz>2.4GHz, pass and The margin is no more margin)

Annie_he_1-1714034744011.png

 

If You have any Ideas to fix this issue in 2M TEST? It may cause us fail in the certification. If you have any ideas, please let us know, thanks.

 

Best Regards,

Annie

 

 

0 Kudos
Reply
3 Replies

1,990 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for contacting NXP support.

Can you please help me with the following information:

  • Are you using an EVK or this is a custom board?
  • Are you using any example from the SDK?
    • What SDK version are you currently using
    • What MCUXpresso version
    • If you are using an SDK example did you perform any changes on the example?

Please let me know this information.

0 Kudos
Reply

1,982 Views
Annie_he
Contributor III

Hi,

   We using custom boards

   SDK version: SDK_2_12_5_KW45B41Z-EVK

   MCUXpresso version: 11.8.0_1165

   FW: connctivity_test

   and We set XtalTrim=26 in SDK example as below:

Annie_he_1-1714101714108.png

    hope your support, thanks

 

   Best Regards,

   Annie

 

 

0 Kudos
Reply

1,929 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you in advance for the response. I will comment this query with our internal team, as we do not have many information regarding the Power certifications. I will be back with some information.

0 Kudos
Reply