Zigbee JN5180

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee JN5180

2,344 Views
berniecheah
Contributor I

Hi,

I understand JN5180 has not been released. But is it possible to use Zigbee and BLE concurrently with the stack for JN5180? Meaning they both run together.

In addition, do you have stack that supports concurrently role for BLE (both central and peripheral role running together? Is KW series able to support this feature?

0 Kudos
Reply
1 Reply

2,078 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

As you mention the JN5180 has not been release and there is no information about it available.

About the KW it is possible using the KW41Z as it supports two connections, I can recommend you to take a look at this thread A view on Bluetooth Low Energy stack roles  

 Best Regards,

Estephania

0 Kudos
Reply