ZPSConfig error - ZigBee 3.0 v.1745

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ZPSConfig error - ZigBee 3.0 v.1745

3,477 次查看
NestorFernandes
Contributor II

I just installed the new JN-SW-4170.v.1745 package and then I tried to compile my project before starting any code adjustment. It seems that the ZPSConfig tool has an internal error:

Building numbered PDM IDs version ...
JENNIC_MAC is Mini MAC shim
JENNIC_MAC_PLATFORM is SOC
Cleaning previous compilation
Assembling irq_JN516x.S
Assembling portasm_JN516x.S
Compiling port_JN516x.c
Configuring the PDUM
PDUMConfig - PDU Manager Configuration Tool v1.1.0 Build 90693

Done.

Compiling pdum_gen.c
Assembling pdum_apdu.S
Configuring the Zigbee Protocol Stack
ZPSConfig - Zigbee Protocol Stack Configuration Tool v1.3.0 Build 91152M

Traceback (most recent call last):
File "ZPSConfig.py", line 2897, in <module>
File "ZPSConfig.py", line 1868, in outputC
UnboundLocalError: local variable 'tempinterface' referenced before assignment
make: *** [../../WIED_R_Router/Source/zps_gen.c] Error 255

Has anyone ever seen that error message?

Does it have to do with the new MacInterfaceList reference?

标记 (2)
0 项奖励
回复
4 回复数

3,131 次查看
dheerajsawant
Contributor V

Hello Sir,

I am using AN-1229 ZP_Application_Templates.

I am also facing same problem. some times its work correctly else zps_gen.c files started showing error.

i am getting all the time below errors please help me to make it successfully.

File "ZPSConfig.py", line 2897, in <module>
File "ZPSConfig.py", line 1868, in outputC

I ALSO ATTACHED FILE PLEASE HAVE A LOOK ON IT.zpsFileError.png

Waiting for your reply.

Thank You 

0 项奖励
回复

3,131 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Could you please add this information in a new post so we can track it down as a different issue from the original? 

Regards, 
Estephania 

0 项奖励
回复

3,131 次查看
charmisuchak
Contributor I

Hi,

I am also facing this same issue while compiling JNAN-1220. Can you please provide the details about how did you resolve this issue?. I tried to search the MacInterfaceList  as suggested but it was inside some node and java files. 

0 项奖励
回复

3,131 次查看
NestorFernandes
Contributor II

Confirmed: if there is no MacInterface defined inside the MacInterfaceList entry, the program will issue that error and crash(?!?).

It could be a little bit more user friendly and give a warning or an error message saying what is missing.

Case solved.