ZPS_eAplZdoJoinNetwork return 194(0xC2)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ZPS_eAplZdoJoinNetwork return 194(0xC2)

2,433件の閲覧回数
jason525
Contributor I

hi,

      Sometimes I get “API failed in vEZ_JoinSavedNetwork 194” message when device attempt to call ZPS_eAplZdoJoinNetwork within  vEZ_JoinSavedNetwork to join network , sometimes it can join the network, have anyone know the reason of this issue?

      I have change the backoff time before the appearance of this issue.

Thanks for any answer.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,232件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jason,

The 0xC2 means Request cannot be processed.

If the case of failure, the device can attempt another join by calling ZPS_eAplZdoJoinNetwork() with a different result reported in the ZPS_EVENT_NWK_DISCOVERY_COMPLETE event

Do you have this issue constant?

Best Regards,

Mario

0 件の賞賛
返信

2,232件の閲覧回数
jason525
Contributor I

Hi, Mario

No, it only happened when the firmware is first download. if download again the issue will disappear.

Best Regards,

Jason

0 件の賞賛
返信