Wandboard USB Bluetooth connectivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wandboard USB Bluetooth connectivity

1,780 Views
markrush
Contributor I

Hello,

I am using the wandboard dual with the freescale yocto os as a reference platform for a new product.

I'm having some issues bringing up a Bluetooth USB dongle.

My base recipe was 'fsl-image-multimedia-full'.  I added all of the Bluez recipes I could find.  They include:

bluez5

bluez5-dbg

bluez5-dev

bluez5-testtools

libasound-module-bluez

Unfortunately, even with these recipes included, I seem to have very little in the way of bluetooth tools.

I am trying to pair with a bluetooth audio streaming device, but an having very little luck.

I have gotten this far:

rfkill list         (correctly finds devices)

rfkill unblock 2  (unblocks the correct device)

hciconfig hci0 up (brings up the correct device)

hciconfig hci0 name xxxx (correctly changes the name)

hcitool scan  (Can see available devices)

hcitool cc my_phone 

At this point, after a timeout, I get 'Can't create connection: Input/output error'

Does anyone have any insight into this?  Unfortunately, I have very little experience with Bluetooth.

Any help would be appreciated.

Mark

0 Kudos
Reply
0 Replies