Unable to program flash on TWR-KW24D512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to program flash on TWR-KW24D512

2,048 Views
calvinjohnson-b
NXP Employee
NXP Employee

While trying to flash twrkw24d512_thread_router_eligible_device on  TWR-KW24D512, I'm getting an error complaining "protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set and mass erase is disabled". Not sure what can be done. Please help.twr_kw24_flash_protect.jpg

0 Kudos
Reply
1 Reply

1,820 Views
calvinjohnson-b
NXP Employee
NXP Employee

The issue was with the connector used. Problem resolved after installing driver from P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...  

USB was used to debug.