USB-KW40Z PCAP IF: No interface Available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB-KW40Z PCAP IF: No interface Available

2,108 Views
juangonzalez
Contributor I

USB-KW40Z

Kinetis Protocol Analyzer Adapter does not show an interface Available to be able to do WireShark

PCAP IF: No interface Available

Options for fixing this?

Labels (1)
0 Kudos
Reply
1 Reply

1,819 Views
antonioconcio
NXP Employee
NXP Employee

Hello,

Could you please try running it with admin rights? If it doesn't work yet, I suggest uninstalling it and then run the setup file with admin rights.

Cheers,

Antonio

0 Kudos
Reply