USB-KW24D512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB-KW24D512

2,179 Views
salah
Contributor III

Hi

I have 2 TWR-KW2x broad. For my experiment I need couple more. Can I use USB-KW24D512 as a TX, RX node instead buying another TWR-KW2x ? As an example if I would like to perform dual pan testing, as per instruction I am required 3 TWR-KW2x board to perform the demo. Can I use USB-KW24D512 instead ?

Any answer would be highly appreciated.

Thanks,
Salah

Tags (2)
1 Reply

2,005 Views
AngelC
Senior Contributor I

Dear Salah,

You could always use the USB-KW24D512 board to load BeeKit solutions. The Beekit new project’s wizard will let you choose the target board, including USB-KW24D512. Please just notice some demos will work differently since the dongle does not have some features such as many buttons, LEDs, etc. The same fact should be taken in consideration in case you want to develop a custom solution.

Regards,

AngelC