Thread statck with KW41Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Thread statck with KW41Z

3,121件の閲覧回数
sensenthuran
Contributor IV

Is that possible to concurrently run KW41Z as  BLE (iBeacon) device and Thread Border Router ?

ラベル(4)
タグ(2)
1 返信

2,009件の閲覧回数
jc_pacheco
NXP Employee
NXP Employee

Hello Sen,

Yes, this will be possible on KW41. Just keep in mind that that since there is only one transceiver, it will need to switch back and forth between BLE and Thread modes. Because of this, there is a chance to miss packets sent over the air when both technologies need to run simultaneously.

Additional KW41Z info can be found at:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/w-s...